Hello,
I have to route a LPDDR4 on an IMX8MPlus and I find contradictory information about line impedance.
In the hardware developer's guide, there is:
- All single-ended signals, unless specified: 50 Ω Single-ended.
- DDR DQS/CLK, PCIe TX/RX data pairs and reference clock: 85 Ω Differential.
And in the memory application note (from ISSI):
- Clock: 70 Ω Differential.
- ADD/CMD/CTRL: 40 Ω
- DQ: 50 Ω
- DQS: 83 Ω Differential
Do you have any recommandations ?
Regards,
Jérôme