limit filters flexcan imx6q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

limit filters flexcan imx6q

1,518件の閲覧回数
vijayraisinghan
Contributor II

Hi,

I am using iMX6Q with has Flexcan Controller, I have some questions :
First, correct me if I am wrong, CAN FD is not supported in iMX6Q (according to this Which processor supports CAN-FD in i.MX6 series?)

However, since the iMX6Q is using Flexcan Controller FlexCAN Controller|NXP, which support "Full implementation of CAN FD", why does iMX6Q not support CAN FD ? Is it hardware limitation ?

Also, what is the upper limit for filters that can be applied using Flexcan linux driver ?

Thanks

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,403件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vijay

>why does iMX6Q not support CAN FD ? Is it hardware limitation ?

yes

 

>Also, what is the upper limit for filters that can be applied using Flexcan linux driver ?

could you clarify question as there are many "filters" description in Reference Manual.

Just for reference attached Linux Manual Chapter 37 FlexCAN Driver gives description of

flexcan driver.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信