libgpuperfcnt can't be fetched from lgfiles link

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

libgpuperfcnt can't be fetched from lgfiles link

1,316 Views
ChristianPrather
Contributor II

Description

 

Hello, when attempting to add the gputop and libgpuperfcnt bitbake files to my Yocto image from https://github.com/nxp-imx/meta-imx/tree/kirkstone-5.15.71-2.2.0/meta-sdk/recipes-graphics/libgpuper... it appears that the link in the bb file is broken.

I am assuming that this is due to a server change? Hoping to get advice on the correct link to update the recipe file. 

 

Error


libgpuperfcnt-6.4.3.p4.6-r0 do_fetch: Failed to fetch URL https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//libgpuperfcnt-6.4.3.p4.6-aarch64-fb.bin;fsl-eula=true;nam..., attempting MIRRORS if available

Seems like there is a missing bin in the lgfiles dir or the link is incorrect.

 

Board

imx8mq

 

Related Issues:

0 Kudos
Reply
6 Replies

1,278 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @ChristianPrather 

Currrently, i am working with L6.1. So i test if the server can work and then it can work with NXP yocto:

~/imx-yocto-bsp$ bitbake libgpuperfcnt
/usr/lib/python3/dist-packages/html5lib/_trie/_base.py:3: DeprecationWarning: Using or importing the ABCs from 'collections' instead of                   from 'collections.abc' is deprecated since Python 3.3, and in 3.10 it will stop working
  from collections import Mapping
Loading cache: 100% |###################################################################################################| Time: 0:00:01
Loaded 4973 entries from dependency cache.
Parsing recipes: 100% |#################################################################################################| Time: 0:00:01
Parsing of 3353 .bb files complete (3351 cached, 2 parsed). 4975 targets, 569 skipped, 3 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION           = "2.2.0"
BUILD_SYS            = "x86_64-linux"
NATIVELSBSTRING      = "universal"
TARGET_SYS           = "aarch64-poky-linux"
MACHINE              = "imx8mqevk"
DISTRO               = "fsl-imx-wayland"
DISTRO_VERSION       = "6.1-langdale"
TUNE_FEATURES        = "aarch64 armv8a crc crypto"
TARGET_FPU           = ""
meta
meta-poky            = "HEAD:b50f718e4cb73214e7ad298484ecdadd6cfeb866"
meta-oe
meta-multimedia
meta-python          = "HEAD:c354f92778c1d4bcd3680af7e0fb0d1414de2344"
meta-freescale       = "HEAD:09c47379218167dda9fb0098129909a667fea2ec"
meta-freescale-3rdparty = "HEAD:96c1f6a6c2cad246687cd695e0873fcc6cdde935"
meta-freescale-distro = "HEAD:1069c2f210b18cd707a4d8a82140a684a42a4ff6"
meta-bsp
meta-sdk
meta-ml
meta-v2x             = "HEAD:d13ade4fdaf536ba7d2db34420755fd23e8736c8"
meta-nxp-demo-experience = "HEAD:c057a681cf11923b22e16b9cdb0ad2b9187eced2"
meta-arm
meta-arm-toolchain   = "HEAD:025124814e8676e46d42ec5b07220283f1bdbcd0"
meta-chromium        = "HEAD:e232c2e21b96dc092d9af8bea4b3a528e7a46dd6"
meta-clang           = "HEAD:22f1cc330d3501923d2dc27cd3fc424c69c3a73a"
meta-gnome
meta-networking
meta-filesystems     = "HEAD:c354f92778c1d4bcd3680af7e0fb0d1414de2344"
meta-qt6             = "HEAD:4f7d02004cd78f0fca77489deb7487bfb301ea36"
meta-parsec
meta-tpm             = "HEAD:2aa48e6f4e519abc7d6bd56da2c067309a303e80"
meta-virtualization  = "HEAD:8857b36ebfec3d548755755b009adc491ef320ab"

Initialising tasks: 100% |##############################################################################################| Time: 0:00:01
Sstate summary: Wanted 61 Local 0 Mirrors 0 Missed 61 Current 258 (0% match, 80% complete)
NOTE: Executing Tasks
NOTE: Tasks Summary: Attempted 1242 tasks of which 1124 didn't need to be rerun and all succeeded.

 

0 Kudos
Reply

1,232 Views
ChristianPrather
Contributor II

@Zhiming_Liu 

Sorry for the delay, got pulled onto some other projects at work.

I tried the recipe listed in the L6.1 release https://github.com/nxp-imx/meta-imx/blob/langdale-6.1.1-1.0.0/meta-sdk/recipes-graphics/libgpuperfcn... however it still fails to find the aarch64 link.

It appears this is a dead link. Can you confirm that libgpuperfcnt-6.4.11.p1.0-aarch64-fb.bin is on the lgfile server?

 

Error 

libgpuperfcnt-6.4.11.p1.0-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//libgpuperfcnt-6.4.11.p1.0-aarch64-fb.bin;fsl-eula=true;na...')

0 Kudos
Reply

1,195 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @ChristianPrather 

Only exists https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//libgpuperfcnt-6.4.11.p1.0-aarch64-wayland.bin

 

 

~/imx-yocto-bsp/build-8mp$ bitbake libgpuperfcnt -c fetch
/usr/lib/python3/dist-packages/html5lib/_trie/_base.py:3: DeprecationWarning: Using or importing the ABCs from 'collections' instead of from 'collections.abc' is deprecated since Python 3.3, and in 3.10 it will stop working
  from collections import Mapping
Loading cache: 100% |#########################################################################| Time: 0:00:00
Loaded 4967 entries from dependency cache.
Parsing recipes: 100% |#######################################################################| Time: 0:00:02
Parsing of 3352 .bb files complete (3345 cached, 7 parsed). 4974 targets, 552 skipped, 4 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION           = "2.2.0"
BUILD_SYS            = "x86_64-linux"
NATIVELSBSTRING      = "universal"
TARGET_SYS           = "aarch64-poky-linux"
MACHINE              = "imx8mp-lpddr4-evk"
DISTRO               = "fsl-imx-wayland"
DISTRO_VERSION       = "6.1-langdale"
TUNE_FEATURES        = "aarch64 armv8a crc crypto"
TARGET_FPU           = ""
meta
meta-poky            = "HEAD:b50f718e4cb73214e7ad298484ecdadd6cfeb866"
meta-oe
meta-multimedia
meta-python          = "HEAD:c354f92778c1d4bcd3680af7e0fb0d1414de2344"
meta-freescale       = "HEAD:09c47379218167dda9fb0098129909a667fea2ec"
meta-freescale-3rdparty = "HEAD:96c1f6a6c2cad246687cd695e0873fcc6cdde935"
meta-freescale-distro = "HEAD:1069c2f210b18cd707a4d8a82140a684a42a4ff6"
meta-bsp
meta-sdk
meta-ml
meta-v2x             = "HEAD:d13ade4fdaf536ba7d2db34420755fd23e8736c8"
meta-nxp-demo-experience = "HEAD:c057a681cf11923b22e16b9cdb0ad2b9187eced2"
meta-arm
meta-arm-toolchain   = "HEAD:025124814e8676e46d42ec5b07220283f1bdbcd0"
meta-chromium        = "HEAD:e232c2e21b96dc092d9af8bea4b3a528e7a46dd6"
meta-clang           = "HEAD:22f1cc330d3501923d2dc27cd3fc424c69c3a73a"
meta-gnome
meta-networking
meta-filesystems     = "HEAD:c354f92778c1d4bcd3680af7e0fb0d1414de2344"
meta-qt6             = "HEAD:4f7d02004cd78f0fca77489deb7487bfb301ea36"
meta-parsec
meta-tpm             = "HEAD:2aa48e6f4e519abc7d6bd56da2c067309a303e80"
meta-virtualization  = "HEAD:8857b36ebfec3d548755755b009adc491ef320ab"
workspace            = "<unknown>:<unknown>"

Initialising tasks: 100% |####################################################################| Time: 0:00:00
Sstate summary: Wanted 0 Local 0 Mirrors 0 Missed 0 Current 0 (0% match, 0% complete)
NOTE: No setscene tasks
NOTE: Executing Tasks
NOTE: Tasks Summary: Attempted 1 tasks of which 0 didn't need to be rerun and all succeeded.

 

 

 

DEBUG: libgpuperfcnt-6.4.11.p1.0-r0 do_fetch: Fetcher accessed the network with the command /usr/bin/env wget -t 2 -T 30 --passive-ftp -O /home/nxf65025/imx-yocto-bsp/downloads/libgpuperfcnt-6.4.11.p1.0-aarch64-wayland.bin.tmp -P /home/nxf65025/imx-yocto-bsp/downloads/ 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//libgpuperfcnt-6.4.11.p1.0-aarch64-wayland.bin'
DEBUG: libgpuperfcnt-6.4.11.p1.0-r0 do_fetch: Running export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/44813/bus"; export ftp_proxy="http://127.0.0.1:3128"; export FTP_PROXY="http://127.0.0.1:3128"; export https_proxy="http://127.0.0.1:3128"; export HTTPS_PROXY="http://127.0.0.1:3128"; export http_proxy="http://127.0.0.1:3128"; export HTTP_PROXY="http://127.0.0.1:3128"; export PATH="/home/nxf65025/imx-yocto-bsp/build-8mp/tmp/sysroots-uninative/x86_64-linux/usr/bin:/home/nxf65025/imx-yocto-bsp/sources/poky/scripts:/home/nxf65025/imx-yocto-bsp/build-8mp/tmp/work/armv8a-mx8mp-poky-linux/libgpuperfcnt/6.4.11.p1.0-r0/recipe-sysroot-native/usr/bin/aarch64-poky-linux:/home/nxf65025/imx-yocto-bsp/build-8mp/tmp/work/armv8a-mx8mp-poky-linux/libgpuperfcnt/6.4.11.p1.0-r0/recipe-sysroot/usr/bin/crossscripts:/home/nxf65025/imx-yocto-bsp/build-8mp/tmp/work/armv8a-mx8mp-poky-linux/libgpuperfcnt/6.4.11.p1.0-r0/recipe-sysroot-native/usr/sbin:/home/nxf65025/imx-yocto-bsp/build-8mp/tmp/work/armv8a-mx8mp-poky-linux/libgpuperfcnt/6.4.11.p1.0-r0/recipe-sysroot-native/usr/bin:/home/nxf65025/imx-yocto-bsp/build-8mp/tmp/work/armv8a-mx8mp-poky-linux/libgpuperfcnt/6.4.11.p1.0-r0/recipe-sysroot-native/sbin:/home/nxf65025/imx-yocto-bsp/build-8mp/tmp/work/armv8a-mx8mp-poky-linux/libgpuperfcnt/6.4.11.p1.0-r0/recipe-sysroot-native/bin:/home/nxf65025/imx-yocto-bsp/sources/poky/bitbake/bin:/home/nxf65025/imx-yocto-bsp/build-8mp/tmp/hosttools"; export HOME="/home/nxf65025"; /usr/bin/env wget -t 2 -T 30 --passive-ftp -O /home/nxf65025/imx-yocto-bsp/downloads/libgpuperfcnt-6.4.11.p1.0-aarch64-wayland.bin.tmp -P /home/nxf65025/imx-yocto-bsp/downloads/ 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//libgpuperfcnt-6.4.11.p1.0-aarch64-wayland.bin' --progress=dot -v
DEBUG: libgpuperfcnt-6.4.11.p1.0-r0 do_fetch: Python function base_do_fetch finished
DEBUG: libgpuperfcnt-6.4.11.p1.0-r0 do_fetch: Python function do_fetch finishe

 

 

0 Kudos
Reply

1,187 Views
ChristianPrather
Contributor II

Okay so the others are missing then, unless this is intentional not to have support for them anymore? In which case the repo needs to be updated to remove them. Is there a reason they are not available anymore?

0 Kudos
Reply

1,166 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

The file name has changed to libgpuperfcnt-6.4.11.p1.0-arm-fb.bin

You can find information in this file:https://github.com/nxp-imx/meta-imx/blob/langdale-6.1.1-1.0.0/SCR-6.1.1-1.0.0.txt

0 Kudos
Reply

1,264 Views
ChristianPrather
Contributor II

Okay thanks for getting back to me, I will check with the new recipe however looking at the diff between them I notice that the SRC I am using (aarch64-fb) is unchanged so I don't expect it to have different results?

Ill check this weekend and update any results here.

0 Kudos
Reply