libgpuperfcnt-6.4.3.p1.4 can't be fetched in Yocto Zeus imx-5.4.70-2.3.2.xml

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

libgpuperfcnt-6.4.3.p1.4 can't be fetched in Yocto Zeus imx-5.4.70-2.3.2.xml

2,511 Views
richard_hu
Senior Contributor I

Hello, NXP team:

 

We encounter build failure on Yocto Zeus ( imx-5.4.70-2.3.2 branch).

The error message shows "ERROR: libgpuperfcnt-6.4.3.p1.4-r0 do_fetch: Fetcher failure for URL: 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/libgpuperfcnt-6.4.3.p1.4-arm-x11.bin;fsl-eula=true;name=ar...'. Unable to fetch URL from any source.
"

Steps:

# repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-zeus -m imx-5.4.70-2.3.2.xml
# repo sync -j8
# DISTRO=fsl-imx-x11 MACHINE=imx6dlsabresd source imx-setup-release.sh -b build-x11-imx6dlsabresd
# bitbake imx-image-full

 

Error message:


WARNING: libgpuperfcnt-6.4.3.p1.4-r0 do_fetch: Failed to fetch URL https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/libgpuperfcnt-6.4.3.p1.4-arm-x11.bin;fsl-eula=true;name=ar..., attempting MIRRORS if available
ERROR: libgpuperfcnt-6.4.3.p1.4-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; unset _PYTHON_SYSCONFIGDATA_NAME; export PATH="/home/jenkins/workspace/yocto-zeus_5.4.70-2.3.2_NXP_official/sources/poky/scripts:/home/jenkins/workspace/yocto-zeus_5.4.70-2.3.2_NXP_official/build-x11-imx6dlsabresd/tmp/work/cortexa9t2hf-neon-mx6qdl-poky-linux-gnueabi/libgpuperfcnt/6.4.3.p1.4-r0/recipe-sysroot-native/usr/bin/arm-poky-linux-gnueabi:/home/jenkins/workspace/yocto-zeus_5.4.70-2.3.2_NXP_official/build-x11-imx6dlsabresd/tmp/work/cortexa9t2hf-neon-mx6qdl-poky-linux-gnueabi/libgpuperfcnt/6.4.3.p1.4-r0/recipe-sysroot/usr/bin/crossscripts:/home/jenkins/workspace/yocto-zeus_5.4.70-2.3.2_NXP_official/build-x11-imx6dlsabresd/tmp/work/cortexa9t2hf-neon-mx6qdl-poky-linux-gnueabi/libgpuperfcnt/6.4.3.p1.4-r0/recipe-sysroot-native/usr/sbin:/home/jenkins/workspace/yocto-zeus_5.4.70-2.3.2_NXP_official/build-x11-imx6dlsabresd/tmp/work/cortexa9t2hf-neon-mx6qdl-poky-linux-gnueabi/libgpuperfcnt/6.4.3.p1.4-r0/recipe-sysroot-native/usr/bin:/home/jenkins/workspace/yocto-zeus_5.4.70-2.3.2_NXP_official/build-x11-imx6dlsabresd/tmp/work/cortexa9t2hf-neon-mx6qdl-poky-linux-gnueabi/libgpuperfcnt/6.4.3.p1.4-r0/recipe-sysroot-native/sbin:/home/jenkins/workspace/yocto-zeus_5.4.70-2.3.2_NXP_official/build-x11-imx6dlsabresd/tmp/work/cortexa9t2hf-neon-mx6qdl-poky-linux-gnueabi/libgpuperfcnt/6.4.3.p1.4-r0/recipe-sysroot-native/bin:/home/jenkins/workspace/yocto-zeus_5.4.70-2.3.2_NXP_official/sources/poky/bitbake/bin:/home/jenkins/workspace/yocto-zeus_5.4.70-2.3.2_NXP_official/build-x11-imx6dlsabresd/tmp/hosttools"; export HOME="/home/jenkins"; /usr/bin/env wget -t 2 -T 30 --passive-ftp --no-check-certificate -P /home/jenkins/workspace/src/yocto3.0/downloads 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/libgpuperfcnt-6.4.3.p1.4-arm-x11.bin' --progress=dot -v failed with exit code 8, output:
--2021-05-31 02:05:46-- https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/libgpuperfcnt-6.4.3.p1.4-arm-x11.bin
Resolving www.nxp.com (www.nxp.com)... 104.116.5.240
Connecting to www.nxp.com (www.nxp.com)|104.116.5.240|:443... connected.
HTTP request sent, awaiting response... 404 Not Found
2021-05-31 02:05:47 ERROR 404: Not Found.


ERROR: libgpuperfcnt-6.4.3.p1.4-r0 do_fetch: Fetcher failure for URL: 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/libgpuperfcnt-6.4.3.p1.4-arm-x11.bin;fsl-eula=true;name=ar...'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/jenkins/workspace/yocto-zeus_5.4.70-2.3.2_NXP_official/build-x11-imx6dlsabresd/tmp/work/cortexa9t2hf-neon-mx6qdl-poky-linux-gnueabi/libgpuperfcnt/6.4.3.p1.4-r0/temp/log.do_fetch.29625
ERROR: Task (/home/jenkins/workspace/yocto-zeus_5.4.70-2.3.2_NXP_official/sources/meta-imx/meta-sdk/recipes-graphics/libgpuperfcnt/libgpuperfcnt_6.4.3.p1.4.bb:do_fetch) failed with exit code '1'

 

You can easily to replicate this problem by downloading:

https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/libgpuperfcnt-6.4.3.p1.4-arm-x11.bin

The link is invalid.

In "imx-5.4.70-2.3.2" branch, it uses "libgpuperfcnt-6.4.3.p1.0".

The download link is:

https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/libgpuperfcnt-6.4.3.p1.0-arm-x11.bin

And it is valid.
 
So, it looks the problem is caused by "https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/libgpuperfcnt-6.4.3.p1.4-arm-x11.bin" is invalid.
Could you fix the link?
 
Thanks~!!!
 
BR,
 
Richard
 
 
Labels (2)
0 Kudos
Reply
4 Replies

666 Views
timblaktu
Contributor I

Well, if you're NXP, it's not really a problem @sinan since they don't support X11 distro. However, it would be very, very nice if NXP and their upstream hardware (SoM) vendors made it much much more clear and painfully obvious that they only really support `DISTRO=fsl-imx-xwayland` and that any errors you encounter when using another DISTRO (or even changing DISTRO_FEATURES in local conf) _are not expected to work_. This has caused me considerable pain, but it's really a matter of acceptance and moving on to find your own solution. It would be great if there were an open space where real users of these platforms crowd-sourced other distros based on `fsl-imx-xwayland` that were more realistic for minimalist use cases that don't want the kitchen sink installed on their embedded devices. This must be the majority of us, however we don't band together much because the companies we work for keep their yocto code private. It's a shame.

0 Kudos
Reply

2,446 Views
richard_hu
Senior Contributor I

Can anyone in NXP help to fix this problem?

0 Kudos
Reply

2,408 Views
joanxie
NXP TechSupport
NXP TechSupport

X11 isn't supported in 5.4 anymore

0 Kudos
Reply

2,473 Views
sinan
Contributor I

The problem still continues.

0 Kudos
Reply