libbeecrypt_cxx on Yocto1.7 (i.MX6)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

libbeecrypt_cxx on Yocto1.7 (i.MX6)

Jump to solution
1,325 Views
yurirellosa
Contributor IV

Hello,

With the following code below I was able to install beecrypt on the rootfs

IMAGE_INSTALL_append += " \

  beecrypt \

  "

I used the same configuration on Yocto1.5 and libbeecrypt_cxx.so.*** was installed

But on Yocto1.7 there is no library with "cxx". Anyone has information regarding this?

Best Regards

Yuri

Labels (3)
0 Kudos
Reply
1 Solution
1,118 Views
yurirellosa
Contributor IV
0 Kudos
Reply
2 Replies
1,119 Views
yurirellosa
Contributor IV
0 Kudos
Reply
1,118 Views
jimmychan
NXP TechSupport
NXP TechSupport
0 Kudos
Reply