I am trying to compile android 13.0.0_1.2.0 for i.mx8m plus board. I executed these commands :
source ./imx-android-13.0.0_1.2.0/imx_android_setup.sh
source build/envsetup.sh
lunch evk_8mp-userdebug
./imx-make.sh kernel -j4 2>&1 | tee build-log.txt
Please check the detail build log info from build-log.txt in the attachment
key error log is:
LTO vmlinux.o
MODPOST vmlinux.symvers
MODINFO modules.builtin.modinfo
GEN modules.builtin
LD .tmp_vmlinux.btf
ld.lld: error: undefined symbol: __stack_chk_guard
>>> referenced by irq-sun6i-r.c:309 (/home2/xiayan/workspace/leopard/imx-android-13.0.0_1.2.0/android_build/vendor/nxp-opensource/kernel_imx/drivers/irqchip/irq-sun6i-r.c:309)
>>> vmlinux.o:(sun6i_r_intc_init)
>>> referenced by irq-sun6i-r.c:311 (/home2/xiayan/workspace/leopard/imx-android-13.0.0_1.2.0/android_build/vendor/nxp-opensource/kernel_imx/drivers/irqchip/irq-sun6i-r.c:311)
>>> vmlinux.o:(sun6i_r_intc_init)
>>> referenced by irq-sun6i-r.c:0 (/home2/xiayan/workspace/leopard/imx-android-13.0.0_1.2.0/android_build/vendor/nxp-opensource/kernel_imx/drivers/irqchip/irq-sun6i-r.c:0)
>>> vmlinux.o:(sun6i_r_intc_init)
>>> referenced 39331 more times
BTF .btf.vmlinux.bin.o
LD .tmp_vmlinux.kallsyms1
ld.lld: error: undefined symbol: __stack_chk_guard
>>> referenced by irq-sun6i-r.c:309 (/home2/xiayan/workspace/leopard/imx-android-13.0.0_1.2.0/android_build/vendor/nxp-opensource/kernel_imx/drivers/irqchip/irq-sun6i-r.c:309)
>>> vmlinux.o:(sun6i_r_intc_init)
>>> referenced by irq-sun6i-r.c:311 (/home2/xiayan/workspace/leopard/imx-android-13.0.0_1.2.0/android_build/vendor/nxp-opensource/kernel_imx/drivers/irqchip/irq-sun6i-r.c:311)
>>> vmlinux.o:(sun6i_r_intc_init)
>>> referenced by irq-sun6i-r.c:0 (/home2/xiayan/workspace/leopard/imx-android-13.0.0_1.2.0/android_build/vendor/nxp-opensource/kernel_imx/drivers/irqchip/irq-sun6i-r.c:0)
>>> vmlinux.o:(sun6i_r_intc_init)
>>> referenced 39331 more times
make[2]: *** [/home2/xiayan/workspace/leopard/imx-android-13.0.0_1.2.0/android_build/vendor/nxp-opensource/kernel_imx/Makefile:1277: vmlinux] Error 1
make[2]: Leaving directory '/home2/xiayan/workspace/leopard/imx-android-13.0.0_1.2.0/android_build/out/target/product/evk_8mq/obj/KERNEL_OBJ'
make[1]: *** [Makefile:237: __sub-make] Error 2
make[1]: Leaving directory '/home2/xiayan/workspace/leopard/imx-android-13.0.0_1.2.0/android_build/vendor/nxp-opensource/kernel_imx'
make: *** [/home2/xiayan/workspace/leopard/imx-android-13.0.0_1.2.0/android_build/device/nxp/common/build/kernel.mk:197: /home2/xiayan/workspace/leopard/imx-android-13.0.0_1.2.0/android_build/out/target/product/evk_8mq/obj/KERNEL_OBJ/arch/arm64/boot/Image.lz4] Error 2
make: Leaving directory '/home2/xiayan/workspace/leopard/imx-android-13.0.0_1.2.0/android_build'
解決済! 解決策の投稿を見る。
ANDROID_ROOT、CROSS_COMPILE、DISCIMAGE、KERNELDIR was definded with error path。
Problem resolved when I clean them
Hi @xiayanfire
From the error log, it seems telling compile env on your host not set properly. The steps that you shared look fine, but one might need to confirm the step "1. Prepare the build environment for U-Boot and Linux kernel."
Best regards
Harvey
Thanks for your reply.
As the step "1. Prepare the build environment for U-Boot and Linux kernel."
I have set the value of AARCH64_GCC_CROSS_COMPILE and CLANG_PATH
AARCH64_GCC_CROSS_COMPILE=/home2/xiayan/workspace/leopard/imx-android-13.0.0_1.2.0/tools/gcc-arm-10.3-2021.07-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu-
CLANG_PATH=/home2/xiayan/workspace/leopard/imx-android-13.0.0_1.2.0/tools/prebuilt-android-clang/linux-x86
All the environment value is saved in env.txt in the attachment
Best regards
xiayanfire
ANDROID_ROOT、CROSS_COMPILE、DISCIMAGE、KERNELDIR was definded with error path。
Problem resolved when I clean them
I think the version for GCC same as guide be better, and the path for clang is not correct.
Best regards
Havey
I tried the same version for GCC as guide :
ARCH64_GCC_CROSS_COMPILE=/home2/xiayan/workspace/leopard/imx-android-13.0.0_1.2.0/tools/gcc-arm-9.2-2019.12-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu-
But it still shows the same error when I compile the kernel。
That is why I wanted to change the version of gcc to gcc-arm-10.3。
Besides, the path of clang(CLANG_PATH=/home2/xiayan/workspace/leopard/imx-android-13.0.0_1.2.0/tools/prebuilt-android-clang/linux-x86) is correct,because I did not rename the path of clang. The detail info of clang is showed as belong:
/home2/xiayan/workspace/leopard/imx-android-13.0.0_1.2.0/tools/prebuilt-android-clang/linux-x86$ ls -l
total 192
-rw-rw-r-- 1 xiayan xiayan 10907 5月 12 17:31 Android.bp
-rw-rw-r-- 1 xiayan xiayan 4748 5月 12 17:27 BINUTILS_KERNEL_DEPRECATION.md
-rw-rw-r-- 1 xiayan xiayan 12581 5月 12 17:31 BUILD.bazel
-rw-rw-r-- 1 xiayan xiayan 16759 5月 12 17:31 cc_toolchain_config.bzl
-rw-rw-r-- 1 xiayan xiayan 7534 5月 12 17:31 cc_toolchain_constants.bzl
-rw-rw-r-- 1 xiayan xiayan 52500 5月 12 17:31 cc_toolchain_features.bzl
drwxrwxr-x 6 xiayan xiayan 4096 5月 12 17:27 clang-3289846
drwxrwxr-x 12 xiayan xiayan 4096 5月 12 17:31 clang-r416183b
drwxrwxr-x 11 xiayan xiayan 4096 5月 12 17:32 clang-r450784d
drwxrwxr-x 11 xiayan xiayan 4096 5月 12 17:27 clang-r450784e
drwxrwxr-x 5 xiayan xiayan 4096 5月 12 17:32 clang-stable
-rw-rw-r-- 1 xiayan xiayan 2467 5月 12 17:27 CleanSpec.mk
drwxrwxr-x 2 xiayan xiayan 4096 5月 12 17:32 docs
-rw-rw-r-- 1 xiayan xiayan 1244 5月 12 17:27 GCC_4_9_DEPRECATION.md
-rw-rw-r-- 1 xiayan xiayan 623 5月 12 17:29 go.mod
drwxrwxr-x 2 xiayan xiayan 4096 5月 12 17:32 llvm-binutils-stable
-rw-rw-r-- 1 xiayan xiayan 1277 5月 12 17:27 METADATA
-rw-rw-r-- 1 xiayan xiayan 377 5月 12 17:27 OWNERS
drwxrwxr-x 2 xiayan xiayan 4096 5月 12 17:32 profiles
-rw-rw-r-- 1 xiayan xiayan 12220 5月 12 17:31 README.md
-rw-rw-r-- 1 xiayan xiayan 7017 5月 12 17:27 RELEASE_NOTES.md
drwxrwxr-x 2 xiayan xiayan 4096 5月 12 17:32 soong
/home2/xiayan/workspace/leopard/imx-android-13.0.0_1.2.0/tools/prebuilt-android-clang/linux-x86$ git status
HEAD detached at 0fc0715d9
nothing to commit, working tree clean
I think that I had set the correct path of AARCH64_GCC_CROSS_COMPILE and CLANG_PATH。
Is there any other wrong env variant ?
Best regards
xiayanfire
Hope you have followed up the 2.1 Setting up your computer.
if still problems, would suggest to have clean build.
Best regards
Harvey
@Harvey021 Is there other suggestion?
Yes, I have followed up the "2.1 Setting up your computer".
My machine is a x86 physical machine with enough hardware resource.
And I have installed all the packages requested in guide again and again .
But the version of Ubuntu is different, it is 20.04.1 64-bit,not 18.04 64-bit. Does this have any effect?
I can not change the version of this machine, because many other people need to use it.
Best regards
xiayanfire