lcdif_pix_clk_enable

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

lcdif_pix_clk_enable

3,353 次查看
rajkumarmadhani
Contributor I

In my u-boot code  working on LCD . lcdif_pix_clk is not running .

these are clock controlling registers.

Anything  am i missing in clock configuration  ?

     /* LCDIF AXI clk from PFD_400M, set to 396/2 = 198MHz */
    reg = readl(CCM_BASE_ADDR + CLKCTL_CSCDR3);
    reg &= ~0x7C000;
    reg |= (0x1 << 16) | (1 << 14);     //reg = 0x00014000
    writel(reg, CCM_BASE_ADDR + CLKCTL_CSCDR3);

    /* LCDIF AXI clk enable */
    reg = readl(CCM_BASE_ADDR + CLKCTL_CCGR3);
    reg |= 0x00C0;
    writel(reg, CCM_BASE_ADDR + CLKCTL_CCGR3);

    /* LCDIF PIX clk from PFD_540M, set to 540/4/5 = 27MHz */
    reg = readl(CCM_BASE_ADDR + CLKCTL_CSCDR2);
    reg &= ~0x0FFF;
    reg |= (0x5 << 6) | (1 << 5);
    writel(reg, CCM_BASE_ADDR + CLKCTL_CSCDR2);

    /* POST DIVIDET for lcdif pix clk */
    reg = readl(CCM_BASE_ADDR + CLKCTL_CSCMR1);
    reg &= ~0x00700000;
    reg |= (0x5 << 20);
    writel(reg, CCM_BASE_ADDR + CLKCTL_CSCMR1);

    /* LCDIF PIX clk enable */
    reg = readl(CCM_BASE_ADDR + CLKCTL_CCGR3);
    reg |= 0x03C0;
    writel(reg, CCM_BASE_ADDR + CLKCTL_CCGR3);
标签 (1)
0 项奖励
回复
5 回复数

2,436 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Rajkumar

also one needs to set correct iomux settings for clk pin and

initialize eLCDIF (perform SFTRST,CLKGATE), please check

sect.21.4.5 Initializing the eLCDIF, 21.5 Behavior During Reset,

IMX6SLRM ,  eLCDIF examples in i.MX 6Series Platform SDK

Bare-metal SDK.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,436 次查看
shefft
Contributor IV

2

Hi, a follow up question as I'm also trying to use the LCDIF.  The terminology is not consistent in the manual for the imx6 SDL.  There is some mention of the LCDIF (not the eLCDIF) but in conjunction with the PXP.  Are they one and same?  In other words, to generate the lcdif_clk do I need to set up the PXP registers?

0 项奖励
回复

2,436 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Tyler

yes LCDIF and eLCDIF is the same.

Regarding settings for eLCDIF I think

i.MX 6Series Platform SDK is best option.

Best regards

igor

0 项奖励
回复

2,436 次查看
shefft
Contributor IV

1

We were able to resolve the issue by returning to using IPU1 instead.

0 项奖励
回复

2,436 次查看
shefft
Contributor IV

2

To clarify, I'm using a Solo.  Do you have a dev guide that covers all the needed LCDIF settings?  The only relevant registers I can find are:

CSCDR2

CSCDR3

CCOSR?

CCGR3

pads:

   NEW_PAD_CTRL(MX6PAD(DI0_DISP_CLK__LCDIF_CLK), DISP_PAD_CTRL),

   NEW_PAD_CTRL(MX6PAD(DI0_PIN15__LCDIF_ENABLE), DISP_PAD_CTRL),

   NEW_PAD_CTRL(MX6PAD(DI0_PIN2__LCDIF_HSYNC), DISP_PAD_CTRL),

   NEW_PAD_CTRL(MX6PAD(DI0_PIN3__LCDIF_VSYNC), DISP_PAD_CTRL),

   NEW_PAD_CTRL(MX6PAD(DISP0_DAT0__LCDIF_DAT_0), DISP_PAD_CTRL),

   NEW_PAD_CTRL(MX6PAD(DISP0_DAT1__LCDIF_DAT_1), DISP_PAD_CTRL),

   NEW_PAD_CTRL(MX6PAD(DISP0_DAT2__LCDIF_DAT_2), DISP_PAD_CTRL),

    NEW_PAD_CTRL(MX6PAD(DISP0_DAT3__LCDIF_DAT_3), DISP_PAD_CTRL),

    NEW_PAD_CTRL(MX6PAD(DISP0_DAT4__LCDIF_DAT_4), DISP_PAD_CTRL),

    NEW_PAD_CTRL(MX6PAD(DISP0_DAT5__LCDIF_DAT_5), DISP_PAD_CTRL),

    NEW_PAD_CTRL(MX6PAD(DISP0_DAT6__LCDIF_DAT_6), DISP_PAD_CTRL),

    NEW_PAD_CTRL(MX6PAD(DISP0_DAT7__LCDIF_DAT_7), DISP_PAD_CTRL),

    NEW_PAD_CTRL(MX6PAD(DISP0_DAT8__LCDIF_DAT_8), DISP_PAD_CTRL),

    NEW_PAD_CTRL(MX6PAD(DISP0_DAT9__LCDIF_DAT_9), DISP_PAD_CTRL),

    NEW_PAD_CTRL(MX6PAD(DISP0_DAT10__LCDIF_DAT_10), DISP_PAD_CTRL),

    NEW_PAD_CTRL(MX6PAD(DISP0_DAT11__LCDIF_DAT_11), DISP_PAD_CTRL),

    NEW_PAD_CTRL(MX6PAD(DISP0_DAT12__LCDIF_DAT_12), DISP_PAD_CTRL),

    NEW_PAD_CTRL(MX6PAD(DISP0_DAT13__LCDIF_DAT_13), DISP_PAD_CTRL),

    NEW_PAD_CTRL(MX6PAD(DISP0_DAT14__LCDIF_DAT_14), DISP_PAD_CTRL),

    NEW_PAD_CTRL(MX6PAD(DISP0_DAT15__LCDIF_DAT_15), DISP_PAD_CTRL),

    NEW_PAD_CTRL(MX6PAD(DISP0_DAT16__LCDIF_DAT_16), DISP_PAD_CTRL),

    NEW_PAD_CTRL(MX6PAD(DISP0_DAT17__LCDIF_DAT_17), DISP_PAD_CTRL),

    NEW_PAD_CTRL(MX6PAD(DISP0_DAT18__LCDIF_DAT_18), DISP_PAD_CTRL),

0 项奖励
回复