Hello everyone,
I am using imx6ulevk eavaluation kit. I am using yocto following L4.9.88_2.0.0 user guide.
My evaluation kit has lcd. I want to understand its initialization routine.
Could someone please help me with reg address in device tree
| lcdif: lcdif@21c8000 { | |
| compatible = "fsl,imx6ul-lcdif", "fsl,imx28-lcdif"; | |
| reg = <0x021c8000 0x4000>; | |
| interrupts = <GIC_SPI 5 IRQ_TYPE_LEVEL_HIGH>; | |
| clocks = <&clks IMX6UL_CLK_LCDIF_PIX>, | |
| <&clks IMX6UL_CLK_LCDIF_APB>, | |
| <&clks IMX6UL_CLK_DUMMY>; | |
| clock-names = "pix", "axi", "disp_axi"; | |
status = "disabled"; } | |
where is the reg address 0x021c8000 defined ? In reference manual or user guide.
How can I know interrupts = <GIC_SPI 5 IRQ_TYPE_LEVEL_HIGH> is defined for lcd?
Regards,
Asma
Solved! Go to Solution.
Hi Asma
one can look at uboot/board/freescale/mx6ul_14x14_evk/mx6ul_14x14_evk.c
mx6ul_14x14_evk.c\mx6ul_14x14_evk\freescale\board - uboot-imx - i.MX U-Boot
in linux sect.6.3.4 ELCDIF Frame Buffer attached Linux Manual.
Right, reg address 0x021c8000 and interrupts are defined in Reference Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
Thank you for the reply. I checked in the above pdf and also IMX6ULRM pdf, I didnt find any address for LCD. If you know can you please specify line number.
Regards,
Asma
Thank you igorpadykov, my bad. I was directly trying to search that address.