latest VPU library for LTIB ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

latest VPU library for LTIB ?

544 Views
allen_kim1
Contributor I

Dear All

Our customer want latest VPU library for LTIB enviroment

Project started with LTIB enviroment and project is almost completed except this issue.

this issue is related with encoding(vpu) but This issue is not occured on YOCTO env

I heard that there are big diffenent between  vpu library on yocto version and vpu library on LTIB version

They Cannot convert LTIB to YOCTO (no time , just one issue and etc...)

We need latest vpu library on LTIB enviroment

Could anybody help us ?

Thanks in advance

Labels (5)
0 Kudos
2 Replies

403 Views
Henry_p
NXP Employee
NXP Employee

Created another DI in MPU support page to escalate this issue.

VPU update for ltib 3.0.35_4.1.0

0 Kudos

403 Views
igorpadykov
NXP Employee
NXP Employee

Hi Allen

what file name do you mean by "vpu library",

I think latest ltib version is L3.0.35_4.1.0., one can look at

Board Support Packages (38)

i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files (REV L3.0.101_4.1.1.)

Codecs and other Algorithms (3)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

or create service request for obtaining specific file.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos