l contact the board(i.MX 8M MiNi EVK) for the first time and l need some help

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

l contact the board(i.MX 8M MiNi EVK) for the first time and l need some help

1,084 Views
tangl
Contributor I

QQ图片20200320170653.pngIt always show me "Error: fail open file: >u-boot-imx8mm-evk-uuu.imx<-[?25h" when l try to executive the command of "uuu.exe uuu-android-mx8mm-evk-emmc.lst", How should l do?

Labels (1)
0 Kudos
Reply
4 Replies

899 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Could you tell me your details steps? Which android version are you using? Are you using the prebuild images?

For the uuu downloading

• On Windows system, open the command line interface in administrator mode. The corresponding command is as
follows:
> .\uuu_imx_android_flash.bat -f imx8mm -a -e -u trusty
When the command above is executed, u-boot-imx8mm-trusty.imx with other default images will be flashed into eMMC
slot a for i.MX 8M Mini EVK.

0 Kudos
Reply

899 Views
tangl
Contributor I

I am using android_p9.0.0_1.0.0-ga_image_8mmevk downloaded from the official website1.png2.png

0 Kudos
Reply

899 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Win10 or Win7 pc are you using? I see your another question also meet the same problem.

0 Kudos
Reply

899 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Does it work now? I see that you are using the i.MX 8M MiNi EVK, but when you download you were using the i.mx8mq images, it's for another board.

.\uuu_imx_android_flash.bat -f imx8mm -a -e

If it still not work contact me.

Have a nice day

Rita

0 Kudos
Reply