kobs-ng open issue: "Unable to dump boot structures"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

kobs-ng open issue: "Unable to dump boot structures"

1,257 次查看
oskar_nilsson
Contributor I

We are trying to use kobs-ng to update u-boot in NAND on a i.MX6UL based board.

Using kobs-ng init to rewrite the whole mtd0 partition works, but using kobs-ng update to update only one bootstream (one copy of u-boot) fails.

Looking at the source on GitHub there is an open issue on the subject:

Unable to dump boot structures · Issue #20 · NXPmicro/imx-kobs · GitHub 

Does NXP have any plans to fix the issue?

标签 (1)
0 项奖励
回复
2 回复数

1,141 次查看
b36401
NXP Employee
NXP Employee

I was told that the update and dump features won’t be merged into the current kobs-ng.
This work is being done in a new port of kobs-ng under u-boot.

0 项奖励
回复

1,141 次查看
b36401
NXP Employee
NXP Employee

Unfortunately the person who works on Kobs-ng is on vacations now.
Please wait a bit.

0 项奖励
回复