kobs-ng open issue: "Unable to dump boot structures"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kobs-ng open issue: "Unable to dump boot structures"

1,303 Views
oskar_nilsson
Contributor I

We are trying to use kobs-ng to update u-boot in NAND on a i.MX6UL based board.

Using kobs-ng init to rewrite the whole mtd0 partition works, but using kobs-ng update to update only one bootstream (one copy of u-boot) fails.

Looking at the source on GitHub there is an open issue on the subject:

Unable to dump boot structures · Issue #20 · NXPmicro/imx-kobs · GitHub 

Does NXP have any plans to fix the issue?

Labels (1)
0 Kudos
Reply
2 Replies

1,187 Views
b36401
NXP Employee
NXP Employee

I was told that the update and dump features won’t be merged into the current kobs-ng.
This work is being done in a new port of kobs-ng under u-boot.

0 Kudos
Reply

1,187 Views
b36401
NXP Employee
NXP Employee

Unfortunately the person who works on Kobs-ng is on vacations now.
Please wait a bit.

0 Kudos
Reply