kobs-ng on i.MX6UL

cancel
Showing results for 
Search instead for 
Did you mean: 

kobs-ng on i.MX6UL

359 Views
yuanba
Contributor I

Hi all,

       I boot device from sd card, then I use kobs-ng flash u-boot.bin/u-boot.imx to mtd, but the device still can not boot from nandflash. what should i do?

       the command: kobs-ng init -v u-boot.imx.

       the firmware was build for booting from mmc/sd, does it matter?

Labels (2)
0 Kudos
1 Reply

73 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Yuan

yes image should be rebuilt, refer to

i.MX 6UltraLite EVK Board Hardware User's Guide sect.2.8 NAND flash

i.MX6ULtraLite Evaluation Kit|Freescale

Note that the data lines of NAND flash are multiplexed with the eMMC and

MicroSD, so they can’t be used at the same time.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos