kobs-ng for imx6 SOLO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kobs-ng for imx6 SOLO

1,901 Views
ao1
Contributor II

I try to put the u-boot into nand using the kobs-ng tool.  The version of the tool is kobs-ng version : [ 1.3 ] git hash (unknown)

Built by Yocto as imx-kobs-3.10.17-1.0.0

I write my u-boot.imx image with NAND support  and the correct DCD data into NAND but it fails to boot. I do see some

activity on the scope on GPMI bus but no proper boot.

Reading imx6 SOLO manual indicates that the FingerPrint for FCB is 0x4E434220, and 0x44424254 DBBT.

However the kobs tool is using other values for imx6:

#define NCB_FINGERPRINT1    0x504d5453  //!< 'STMP'
#define NCB_FINGERPRINT2    0x2042434e  //!< 'NCB<space>' - NAND Control Block
#define NCB_FINGERPRINT3    0x4e494252  //!< 'RBIN' - ROM Boot Image Block - N

#define FCB_FINGERPRINT     0x20424346  //!< 'FCB '
#define FCB_VERSION_1       0x01000000

#define LDLB_FINGERPRINT1   0x504d5453  //!< 'STMP'
#define LDLB_FINGERPRINT2   0x424c444c  //!< 'LDLB' - Logical Device Layout Block
#define LDLB_FINGERPRINT3   0x4c494252  //!< 'RBIL' - ROM Boot Image Block - L

#define DBBT_FINGERPRINT1   0x504d5453  //!< 'STMP'
#define DBBT_FINGERPRINT2_V20x44424254  //!< 'DBBT' - Discovered Bad Block Table.
#define DBBT_FINGERPRINT2   0x54424244  //!< 'DBBT' - Discovered Bad Block Table.
#define DBBT_FINGERPRINT3   0x44494252  //!< 'RBID' - ROM Boot Image Block - D
#define DBBT_VERSION_1      0x01000000

#define LDLB_VERSION_MAJOR   0x0001

#define LDLB_VERSION_MINOR   0x0000

#define LDLB_VERSION_SUB 0x0000

#define TYPICAL_NAND_READ_SIZE          2048

When I write the u-boot I observe different Fingerprints:

root@imx6s:~# kobs-ng init -v -w u-boot.imx                                                                                                                                                                                                                                                                      

it is an IMX6 platform

MTD CONFIG:

  chip_0_device_pnand_erase_nand: attempt to erase a bad block at page 0x00000000

ath = "/dev/mtd0"

  chip_1_device_path = "(null)"

  search_exponent = 2

  data_setup_time = 80

  data_hold_time = 60

  address_setup_time = 25

  data_sample_time = 6

  row_address_size = 3

  column_address_size = 2

  read_command_code1 = 0

  read_command_code2 = 48

  boot_stream_major_version = 1

  boot_stream_minor_version = 0

  boot_stream_sub_version = 0

  ncb_version = 3

  boot_stream_1_address = 0

  boot_stream_2_address = 0

u-boot.imx: verifying using key '00000000000000000000000000000000'

u-boot.imx: is a valid bootstream for key '00000000000000000000000000000000'

mtd: opening: "/dev/mtd0"

NFC geometry :

    ECC Strength   : 8
    Page Size in Bytes : 2112
    Metadata size  : 10
    ECC Chunk Size in byte : 512
    ECC Chunk count    : 4
    Block Mark Byte Offset : 1999
    Block Mark Bit Offset  : 0

====================================================

mtd: opened '/dev/mtd0' - '(null)'

mtd: max_boot_stream_size_in_bytes = 7864320

mtd: boot_stream_size_in_bytes = 510976

mtd: boot_stream_size_in_pages = 250

mtd: #1 0x00100000 - 0x00880000 (0x0017cc00)

mtd: #2 0x00880000 - 0x01000000 (0x008fcc00)

FCB

  m_u32Checksum = 0x00000000

  m_u32FingerPrint = 0x20424346

  m_u32Version = 0x01000000

  m_NANDTiming.m_u8DataSetup = 80

  m_NANDTiming.m_u8DataHold = 60

  m_NANDTiming.m_u8AddressSetup = 25

  m_NANDTiming.m_u8DSAMPLE_TIME = 6

  m_u32PageDataSize = 2048

  m_u32TotalPageSize = 2112

  m_u32SectorsPerBlock = 64

  m_u32NumberOfNANDs = 0

  m_u32TotalInternalDie = 0

  m_u32CellType = 0

  m_u32EccBlockNEccType = 4

  m_u32EccBlock0Size = 512

  m_u32EccBlockNSize = 512

  m_u32EccBlock0EccType = 4

  m_u32MetadataBytes = 10

  m_u32NumEccBlocksPerPage = 3

  m_u32EccBlockNEccLevelSDK = 0

  m_u32EccBlock0SizeSDK = 0

  m_u32EccBlockNSizeSDK = 0

  m_u32EccBlock0EccLevelSDK = 0

  m_u32NumEccBlocksPerPageSDK = 0

  m_u32MetadataBytesSDK = 0

  m_u32EraseThreshold = 0

  m_u32Firmware1_startingPage = 512

  m_u32Firmware2_startingPage = 4352

  m_u32PagesInFirmware1 = 250

  m_u32PagesInFirmware2 = 250

  m_u32DBBTSearchAreaStartAddress = 256

  m_u32BadBlockMarkerByte = 1999

  m_u32BadBlockMarkerStartBit = 0

  m_u32BBMarkerPhysicalOffset = 2048

  m_u32BCHType = 0

  m_NANDTMTiming.m_u32TMTiming2_ReadLatency = 0

  m_NANDTMTiming.m_u32TMTiming2_PreambleDelay = 0

  m_NANDTMTiming.m_u32TMTiming2_CEDelay = 0

  m_NANDTMTiming.m_u32TMTiming2_PostambleDelay = 0

  m_NANDTMTiming.m_u32TMTiming2_CmdAddPause = 0

  m_NANDTMTiming.m_u32TMTiming2_DataPause = 0

  m_NANDTMTiming.m_u32TMSpeed = 0

  m_NANDTMTiming.m_u32TMTiming1_BusyTimeout = 0

  m_u32DISBBM = 0

DBBT

  m_u32Checksum = 0x00000000

  m_u32FingerPrint = 0x54424244

  m_u32Version = 0x01000000

  m_u32DBBTNumOfPages = 0

Firmware: image #0 @ 0x100000 size 0x7d000 - available 0x780000

Firmware: image #1 @ 0x880000 size 0x7d000 - available 0x780000

-------------- Start to write the [ FCB ] -----

mtd: erasing @0:0x0-0x20000

mtd: device 0 fails MEMERASE (0x0 - 0x20000)

mtd: Failed to erase block @0x0

mtd: erasing @0:0x20000-0x40000

mtd: Writing FCB1 [ @0:0x20000 ] (840) *

mtd: erasing @0:0x40000-0x60000

mtd: Writing FCB2 [ @0:0x40000 ] (840) *

mtd: erasing @0:0x60000-0x80000

mtd: Writing FCB3 [ @0:0x60000 ] (840) *

mtd_commit_bcb(FCB): status 1

-------------- Start to write the [ DBBT ] -----

mtd: erasing @0:0x80000-0xa0000

mtd: Writing DBBT0 [ @0:0x80000 ] (800) *

mtd: erasing @0:0xa0000-0xc0000

mtd: Writing DBBT1 [ @0:0xa0000 ] (800) *

mtd: erasing @0:0xc0000-0xe0000

mtd: Writing DBBT2 [ @0:0xc0000 ] (800) *

mtd: erasing @0:0xe0000-0x100000

mtd: Writing DBBT3 [ @0:0xe0000 ] (800) *

mtd_commit_bcb(DBBT): status 0

---------- Start to write the [ u-boot.imx ]----

mtd: Writting u-boot.imx: #0 @0: 0x00100000 - 0x0017d000

mtd: erasing @0:0x100000-0x120000

mtd: erasing @0:0x120000-0x140000

mtd: erasing @0:0x140000-0x160000

mtd: erasing @0:0x160000-0x180000

mtd: The last page is not full : 1024

mtd: We write one page for save guard. *

mtd: Writting u-boot.imx: #1 @0: 0x00880000 - 0x008fd000

mtd: erasing @0:0x880000-0x8a0000

mtd: erasing @0:0x8a0000-0x8c0000

mtd: erasing @0:0x8c0000-0x8e0000

mtd: erasing @0:0x8e0000-0x900000

mtd: The last page is not full : 1024

mtd: We write one page for save guard. *

The FCB and DBBT are:

FCB

  m_u32Checksum = 0x00000000

  m_u32FingerPrint = 0x20424346 ???????????

  m_u32Version = 0x01000000

DBBT

  m_u32Checksum = 0x00000000

  m_u32FingerPrint = 0x54424244 ?????????

  m_u32Version = 0x01000000

When I do a dump I get the following:

kobs-ng dump -v         

it is an IMX6 platform

MTD CONFIG:

  chip_0_device_path = "/dev/mtd0"

  chip_1_device_path = "(null)"

  search_exponent = 2

  data_setup_time = 80

  data_hold_time = 60

  address_setup_time = 25

  data_sample_time = 6

  row_address_size = 3

  column_address_size = 2

  read_command_code1 = 0

  read_command_code2 = 48

  boot_stream_major_version = 1

  boot_stream_minor_version = 0

  boot_stream_sub_version = 0

  ncb_version = 3

  boot_stream_1_address = 0

  boot_stream_2_address = 0

mtd: opening: "/dev/mtd0"

NFC geometry :

    ECC Strength   : 8
    Page Size in Bytes : 2112
    Metadata size  : 10
    ECC Chunk Size in byte : 512
    ECC Chunk count    : 4
    Block Mark Byte Offset : 1999
    Block Mark Bit Offset  : 0

====================================================

mtd: opened '/dev/mtd0' - '(null)'

mtd: partition #0

  type = 4

  flags = 17408

  size = 16777216

  erasesize = 131072

  writesize = 2048

  oobsize = 64

  blocks = 128

mtd: fingerprints mismatch @0:0x0

[0000] 20 28 01 83 38 40 82 04  58 68 83 87 90 a8 05 8c |  (..8@..-Xh......

[0010] e8 10 89 13 78 b9 8e 9f  60 ca 17 b3 d8 83 a6 52 | ....x...-`......R

[0020] 38 4e be 05 10 d2 64 58  48 20 23 5e 58 f2 87 b6 | 8N....dX-H #^X...

[0030] a0 12 ab 14 f8 04 33 cb  98 17 de df 90 1c 11 ab | ......3.-........

[0040] 28 34 ef 8a b8 50 00 36  e0 84 ef c0 98 d5 ef f6 | (4...P.6-........

[0050] 78 5a df b7 10 30 cf ae  88 8a ae 66 98 ba 7d 15 | xZ...0..-...f..}.

[0060] 20 45 2c 7c b8 ff a9 91  d8 44 d6 0d 90 44 80 9f |  E,|....-.D...D..

[0070] 68 89 56 ad f8 cd d6 4c  60 57 2d fa 58 25 04 47 | h.V....L-`W-.X%.G

[0080] b8 7c 31 41 10 a2 35 88  c8 1e 67 c9 d8 c0 9c 51 | .|1A..5.-..g....Q

mtd: fingerprints mismatch @0:0x20000

[0000] d9 fa ff ff 46 43 42 20  00 00 00 01 50 3c 19 06 | ....FCB -....P<..

[0010] 00 00 00 00 00 08 00 00  40 08 00 00 40 00 00 00 | ........-@...@...

[0020] 00 00 00 00 00 00 00 00  00 00 00 00 04 00 00 00 | ........-........

[0030] 00 02 00 00 00 02 00 00  04 00 00 00 0a 00 00 00 | ........-........

[0040] 03 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0050] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0060] 00 00 00 00 00 00 00 00  00 02 00 00 00 11 00 00 | ........-........

[0070] fa 00 00 00 fa 00 00 00  00 01 00 00 cf 07 00 00 | ........-........

[0080] 00 00 00 00 00 08 00 00  00 00 00 00 00 00 00 00 | ........-........

mtd: fingerprints mismatch @0:0x40000

[0000] d9 fa ff ff 46 43 42 20  00 00 00 01 50 3c 19 06 | ....FCB -....P<..

[0010] 00 00 00 00 00 08 00 00  40 08 00 00 40 00 00 00 | ........-@...@...

[0020] 00 00 00 00 00 00 00 00  00 00 00 00 04 00 00 00 | ........-........

[0030] 00 02 00 00 00 02 00 00  04 00 00 00 0a 00 00 00 | ........-........

[0040] 03 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0050] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0060] 00 00 00 00 00 00 00 00  00 02 00 00 00 11 00 00 | ........-........

[0070] fa 00 00 00 fa 00 00 00  00 01 00 00 cf 07 00 00 | ........-........

[0080] 00 00 00 00 00 08 00 00  00 00 00 00 00 00 00 00 | ........-........

mtd: fingerprints mismatch @0:0x60000

[0000] d9 fa ff ff 46 43 42 20  00 00 00 01 50 3c 19 06 | ....FCB -....P<..

[0010] 00 00 00 00 00 08 00 00  40 08 00 00 40 00 00 00 | ........-@...@...

[0020] 00 00 00 00 00 00 00 00  00 00 00 00 04 00 00 00 | ........-........

[0030] 00 02 00 00 00 02 00 00  04 00 00 00 0a 00 00 00 | ........-........

[0040] 03 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0050] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0060] 00 00 00 00 00 00 00 00  00 02 00 00 00 11 00 00 | ........-........

[0070] fa 00 00 00 fa 00 00 00  00 01 00 00 cf 07 00 00 | ........-........

[0080] 00 00 00 00 00 08 00 00  00 00 00 00 00 00 00 00 | ........-........

mtd: NCB0 not found

mtd: fingerprints mismatch @0:0x80000

[0000] 00 00 44 42 42 54 00 00  00 01 00 00 00 00 00 00 | ..DBBT..-........

[0010] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0020] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0030] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0040] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0050] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0060] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0070] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0080] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

mtd: fingerprints mismatch @0:0xa0000

[0000] 00 00 44 42 42 54 00 00  00 01 00 00 00 00 00 00 | ..DBBT..-........

[0010] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0020] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0030] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0040] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0050] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0060] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0070] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0080] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

mtd: fingerprints mismatch @0:0xc0000

[0000] 00 00 44 42 42 54 00 00  00 01 00 00 00 00 00 00 | ..DBBT..-........

[0010] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0020] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0030] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0040] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0050] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0060] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0070] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0080] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

mtd: fingerprints mismatch @0:0xe0000

[0000] 00 00 44 42 42 54 00 00  00 01 00 00 00 00 00 00 | ..DBBT..-........

[0010] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0020] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0030] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0040] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0050] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0060] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0070] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

[0080] 00 00 00 00 00 00 00 00  00 00 00 00 00 00 00 00 | ........-........

mtd: NCB1 not found

mtd: neither NCB1 or NCB2 found ERROR

Unable to load boot structures

root@imx6s:~#

The first FCB stride is damaged because of the bad block at the start, but the

rest should be ok..

I have the feeling that  kobs-ng might not be the right version, or something else has gone wrong ..

Does anyone used kobs-ng on IMX6 SOLO successfully ? Have you seen similar problems?

Thank you

Andreas

Labels (3)
0 Kudos
2 Replies

545 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

The kobs values seem to be correct. Have you checked if the image .imx is with the 0x400 offsset?

Best Regards,

Alejandro

0 Kudos

545 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I have not used kobs-ng for the imx6 SOLO.

I will check the differences in the code first. I will get back to you as soon as I find something.

Best Regards,

Alejandro

0 Kudos