kmalloc() GFP_ATOMIC fails - how to fix?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kmalloc() GFP_ATOMIC fails - how to fix?

1,654件の閲覧回数
ArtyomKamshilin
Contributor II

Hi everyone,

I'm trying to use a third-party driver on an i.MX28 box, and the driver does quite a few kmalloc() calls with GFP_ATOMIC parameter. This call is known to fail when kernel cannot find a reserved memory page for an atomic allocation operation. I tried increasing kernel configuration parameter called CONFIG_SECURITY_DEFAULT_MMAP_MIN_ADDR (also known as “Low address space to protect from user allocation”) from a default value of 4096 to a maximum of 32768 recommended for ARM platforms. It didn't resolve the problem, so:

Question: which parameter should be tweaked to allow kernel a bit more flexibility for atomic page allocations?

Thanks in advance.

/Arty

タグ(2)
0 件の賞賛
返信
0 返答(返信)