kernel crash after local_irq_restore call

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kernel crash after local_irq_restore call

1,366件の閲覧回数
mihaitaivascu
Contributor III

Hello,

    I have a general question about interrupts on imx6ul.

    I am working with bluetooth and have a kernel crash where last call is local_irq_restore.

    I understand that another driver is misbehaving and not disabling interrupts. Is this correct?

    What should I check additionally?

Thanks,

      Mihaita Ivascu

ラベル(1)
0 件の賞賛
返信
1 返信

1,295件の閲覧回数
art
NXP Employee
NXP Employee

Q. I understand that another driver is misbehaving and not disabling interrupts. Is this correct?

A. Yes, this seems to be correct.

Q. What should I check additionally?

A. If the system contains some custom drivers (not only the drivers, included in the basic configuration), check whether they process interrupts and restore from interrupt state correctly.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信