kernel configuration for i.MX8 PCIe cerification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kernel configuration for i.MX8 PCIe cerification

Jump to solution
1,647 Views
m_c
Senior Contributor I

In application note an12444 <http://nxp.com/doc/an12444>, 2.3 test environment said set CONFIG_PCI_IMX8_COMPLIANCE_TEST=y.

But we can't find it in kernel 4.14.98, but found CONFIG_PCI_IMX6_COMPLIANCE_TEST.

Which kernel configuration should we used for PCIe cerification?

Labels (2)
0 Kudos
1 Solution
1,373 Views
Yuri
NXP Employee
NXP Employee

Hello,

   set "CONFIG_PCI_IMX6_COMPLIANCE_TEST=y", and rebuild the kernel image.

Regards,

Yuri.

View solution in original post

0 Kudos
5 Replies
353 Views
Danube
Contributor IV

Hi All,

For i.MX8MP

For 6.1.55 kernel ,

 

Need to add "pcie_phy_tuned=yes" to mmcargs in U-boot

0 Kudos
1,373 Views
jiangyaqiang
Contributor IV

HI m.c:

        Does the PCIE eye pattern test signal come out after "set "CONFIG_PCI_IMX6_COMPLIANCE_TEST=y", and rebuild the kernel image" ? I did the same thing , but no signal.

0 Kudos
1,373 Views
m_c
Senior Contributor I

Yes

0 Kudos
1,373 Views
jiangyaqiang
Contributor IV

HI m.c:

Thanks.

After tested, we found that PCIE1 have the signal but PCIE0 no, but PCIE0 is working for my wifi module.

江亚强

软件工程师

Shenzhen Huameishi Technology Co., Ltd

深圳市华美视科技有限公司

深圳市南山区科苑路6号科技园工业大厦605

Tel:0755-26037882-616

Mail:yaqiang.jiang@huameishi.com

0 Kudos
1,374 Views
Yuri
NXP Employee
NXP Employee

Hello,

   set "CONFIG_PCI_IMX6_COMPLIANCE_TEST=y", and rebuild the kernel image.

Regards,

Yuri.

0 Kudos