issue on emmc with mfgtool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

issue on emmc with mfgtool

2,176 次查看
jingyangxie
Contributor V

Hi,all

     I have a imx6sxbresd board, use mfgtool(linux3.14.52) to download the OS into emmc(emmc4.5),but it failed.the console logged:

error -110 whilst initialising MMC card

anyone kowns?

标签 (2)
0 项奖励
回复
7 回复数

1,961 次查看
igorpadykov
NXP Employee
NXP Employee

Hi  jingyang

one can check if correct dev/mmcblk"x"p"y" was used and

check signals with oscilloscope. Try to test emmc from uboot.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,961 次查看
jingyangxie
Contributor V

Hi,igor

    my emmc is 8G ,but when use mfgtool to download image into it ,the console prints as followed:

   mmc3: new MMC card at address 0001
   mmcblk3: mmc3:0001 16 1.00 GiB

why deos  the volume of emmc which the system check is different from the actual value ?

0 项奖励
回复

1,961 次查看
igorpadykov
NXP Employee
NXP Employee

Hi  jingyang

 

please try to test emmc from uboot, check emmc partitions.

 

Best regards
igor

0 项奖励
回复

1,961 次查看
jingyangxie
Contributor V

Hi,igor

    My board cannot step into uboot

0 项奖励
回复

1,961 次查看
igorpadykov
NXP Employee
NXP Employee

Hi  jingyang

please try to boot from other media, for example sd.

eMMC Partition by U-boot (i.MX53) 

kernel/git/torvalds/linux.git - Linux kernel source tree 

Best regards
igor

1,961 次查看
jingyangxie
Contributor V

Hi,igor

    thans for your patience. I found that the chip was bad, and when I change one ,the issue is solved.

0 项奖励
回复

1,961 次查看
jingyangxie
Contributor V

Hi,igor

    How can I test emmc from uboot,is there operation steps for details?

0 项奖励
回复