issue in Imxdl booting from emmc.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

issue in Imxdl booting from emmc.

471 Views
prasannakulkarni
Contributor IV

Hi all,

We have got imx6s processor custom board... So using config for imx6dl defconfigs for building uboot... But it is not detecting emmc as a boot device... It is taking sd3 as boot device and tells mmc card not found.... Where to set this... can u plz help me.

This board works for 2013.uboot and i could able to flash ics successfully.... But when i try to flash uboot.2017.03 it is stopping at uboot telling mmc card not found no booting device found.... Because it is looking for sdcard in place of emmc. So where to change this in the uboot kindly help...

Labels (3)
0 Kudos
1 Reply

371 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

In our reference design, the SD4 is work for emmc. If the board you design yourself and you need to do porting BSP first.

0 Kudos