issue about imx6 IPU output

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

issue about imx6 IPU output

1,087 Views
宗標廖
Contributor V

Hello Community

We met a problem about imx6 IPU as bellow.

Data path =

imx6 BT 656 capture input, crop size = 720 x 480, capture format = 720 x 480, 60fps progressive

then,

do memory copy to output buffer,

then,

imx6 V4L2 output scaling on /dev/video17, format = 720x480, output cropsize = 1280 x 720, 60fps progressive, output dot clock frequency = 59.03MHz

then we found out that the display image is NG, and the right-most edge area is lost.

We did another test like this:

imx6 BT 656 capture input, crop size = 720 x 480, capture format = 720 x 480, 60fps progressive

then,

do memory copy to output buffer,

then,

imx6 V4L2 output scaling on /dev/video17, format = 720x480, output cropsize = 1080 x 720, 60fps progressive, output dot clock frequency = 59.03MHz

then we found out that the display image occupies the left part of the display area as expected(because the display area is 1280x720), and the right-most edge area is NOT lost.


Is it because of some kind of limitation in IMX6solo IPU capability? How can we overcome this effect?

Best Regards

ZongbiaoLiao

Labels (2)
0 Kudos
Reply
1 Reply

819 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the mx6s reference manual, mx6s can support 720p output.

you don't use vpu, just capture video then output right? could you tell me what's command you use? and any error log file?

0 Kudos
Reply