issue about DirectFB in imx6DL at version 3.14.28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

issue about DirectFB in imx6DL at version 3.14.28

1,390 Views
xiehuijun
Contributor II

I want to use DirectFB for 2D graphical hardware acceleration.but i found a strange problem.

when i use gfxdriver(libdirectfb_gal.so), i run the directfb example "df_andi", there is only 6 FPS and "cpu idle" is 50%, even if i set "no-hardware" in "directfbrc", it is the same.

but if i remove the library(libdirectfb_gal.so),it means using software acceleration, the example will up to 20 FPS and "cpu idle" 60%. why ?

and i have another question:

if i set "fbdev=/dev/fb1" (at the FG not BG), it  will display nothing in screen, but there is no error.

does the "fbdev" must set to "BG" ?

i have tested the example at official image , it was the same result.

additional:

i use buildroot for building filesystem, directfb version is V1.7.4

-----------------------------------------------------------------------------------------

my directfb settings:

# cat /etc/directfbrc

no-cursor

system=fbdev

fbdev=/dev/fb0

mode=1920x1080

depth=32

pixelformat=RGB32

#quiet

#no-hardware

-------------------------------------------------------------------------------------

the log message is below:

# df_andi

(*) Direct/Thread: Started 'SigHandler' (246) [CRITICAL - OTHER/0] <8388608>...

   ~~~~~~~~~~~~~~~~~~~~~~~~~~| DirectFB 1.7.4 |~~~~~~~~~~~~~~~~~~~~~~~~~~

        (c) 2012-2013  DirectFB integrated media GmbH

        (c) 2001-2013  The world wide DirectFB Open Source Community

        (c) 2000-2004  Convergence (integrated media) GmbH

      ----------------------------------------------------------------

(*) DirectFB/Core: Single Application Core. (2016-01-25 07:37)

(*) Direct/Memcpy: Using libc memcpy()

(*) Direct/Thread: Started 'Fusion Dispatch' (247) [MESSAGING - OTHER/0] <8388608>...

(*) Direct/Thread: Started 'VT Switcher' (250) [CRITICAL - OTHER/0] <8388608>...

(*) Direct/Thread: Started 'VT Flusher' (251) [DEFAULT - OTHER/0] <8388608>...

(*) DirectFB/FBDev: Found 'DISP3 BG - DI1' (ID 0) with frame buffer at 0x3c100000, 8100k (MMIO 0x00000000, 0k)

(*) Direct/Thread: Started 'Hotplug with Linux Input' (252) [INPUT - OTHER/0] <8388608>...

(*) DirectFB/Input: Hot-plug detection enabled with Linux Input Driver

(*) Direct/Thread: Started 'Keyboard Input' (253) [INPUT - OTHER/0] <8388608>...

(*) DirectFB/Input: Keyboard 0.9 (directfb.org)

(*) Using the default feature settings.

(*) DirectFB/Graphics: Vivante unknown chip model 1.0 (Vivante)

(*) DirectFB/Core/WM: Default 0.3 (directfb.org)

(*) Direct/Thread: Started 'Genefx' (254) [DEFAULT - OTHER/0] <8388608>...

(*) FBDev/Mode: Setting 1920x1080 RGB32

(*) FBDev/Mode: Switched to 1920x1080 (virtual 1920x1080) at 32 bit (RGB32), pitch 7680

:smileyalert: DirectFB/DirectFBCreate: Setting desktop resolution to 1920x1080 failed!

     -> Using default resolution.

:smileyalert: DirectFB/DirectFBCreate: Setting desktop format failed!

     -> Using default format.

:smileyalert: DirectFB/DirectFBCreate: Setting desktop buffer mode failed!

     -> No virtual resolution support or not enough memory?

        Falling back to system back buffer.

(*) FBDev/Mode: Setting 1920x1080 RGB32

(*) FBDev/Mode: Switched to 1920x1080 (virtual 1920x1080) at 32 bit (RGB32), pitch 7680

(*) Direct/Interface: Loaded 'FT2' implementation of 'IDirectFBFont'.

(*) Direct/Interface: Loaded 'PNG' implementation of 'IDirectFBImageProvider'.

(*) Direct/Interface: Loaded 'JPEG' implementation of 'IDirectFBImageProvider'.

(*) FBDev/Mode: Setting 1920x1080 RGB32

(*) FBDev/Mode: Switched to 1920x1080 (virtual 1920x1080) at 32 bit (RGB32), pitch 7680

----------------------------------------------------------------------------------------------------------------------------

somebody else faced this problem ?

Labels (4)
0 Kudos
Reply
1 Reply

555 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi xie,

This is an issue with libdirectfb_gal, however I do not know if this going to be fixed, Since there is no DirectFB support anymore. I suggest to use Wayland instead.

Regards

0 Kudos
Reply