isp_media_server segmentation fault at VIV_VIDEO_EVENT_SET_CROP or other mmap operations

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

isp_media_server segmentation fault at VIV_VIDEO_EVENT_SET_CROP or other mmap operations

跳至解决方案
272 次查看
r3gl0
Contributor II

I'm currently working with the NXP IMX8MPLUS and trying to enable the ISP for the MT9V024 camera sensor.

My current set up is following:

Yocto core image with IMAGE_INSTALL:append = " kernel-module-isp-vvcam gstreamer1.0 gstreamer1.0-plugins-base gstreamer1.0-plugins-good gstreamer1.0-plugins-bad v4l-utils isp-imx libtinyxml2 media-ctl fmt ".

Linux 5.15.71 Kirkstone
Is a headless build

Externally, I build:

- isp-imx-4.2.2.20.0
- isp-vvcam (lf-5.15.y_2.2.0)
and then I send the generated files to the board.

My current bottle neck is that when I run

gst-launch-1.0 -v v4l2src device=/dev/video0 ! "video/x-raw,format=YUY2,width=752,height=480" ! queue ! videoconvert ! theoraenc ! oggmux ! filesink location=test_image.ogv

isp_media_server crashes in the VIV_VIDEO_EVENT_SET_CROP case. To be more specific it crashes here:

---(source isp-imx-4.2.2.20.0/mediacontrol/daemon/V4l2Event.cpp)--

case VIV_VIDEO_EVENT_SET_CROP: {
ALOGI("VIV_VIDEO_EVENT_SET_CROP"); // I add this for debug.

if (bufMap.find(event.addr) == bufMap.end()) {
bufMap[event.addr] = ::mmap(NULL, VIV_JSON_BUFFER_SIZE,
PROT_READ | PROT_WRITE, MAP_SHARED, eventDevice, event.addr);
}
struct viv_rect *rect = (struct viv_rect *)bufMap[event.addr]; // gdb points at this line.

// It is weird to fail here because v4l2-ctl --all -d /dev/video0 works well (check log)

-----

 

---
It also crashes when I perform any other operation like v4l2-ctl -d 0 -c viv_ext_ctrl='{<id>:<pipeline.s.dwe.onoff>;<enable>:false}'

Here i had heavily modify the code for testing purposes:

case VIV_VIDEO_EVENT_EXTCTRL: {
ALOGI("VIV_VIDEO_EVENT_EXTCTRL: Event received.");
ALOGI("VIV_VIDEO_EVENT_EXTCTRL: event.addr = 0x%llx", (long long)event.addr);
ALOGI("VIV_VIDEO_EVENT_EXTCTRL: eventDevice = %d", eventDevice);
ALOGI("VIV_VIDEO_EVENT_EXTCTRL: VIV_JSON_BUFFER_SIZE = %zu", (size_t)VIV_JSON_BUFFER_SIZE);

{

struct stat st;
if (fstat(eventDevice, &st) == -1) {
perror("fstat failed");
} else {
printf("eventDevice size: %lld bytes\n", (long long)st.st_size);
printf("Trying to mmap at offset: %lld\n", (long long)event.addr);
}
}
{

struct v4l2_requestbuffers req = {0};
req.count = 1;
req.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
req.memory = V4L2_MEMORY_MMAP;

if (ioctl(eventDevice, VIDIOC_REQBUFS, &req) == -1) {
ALOGE("VIDIOC_REQBUFS failed: %s", strerror(errno));
} else {
ALOGI("Requested %u buffers, got %u", req.count, req.count);
}

struct v4l2_buffer buf = {0};
buf.index = 0;
buf.type = V4L2_BUF_TYPE_VIDEO_CAPTURE;
buf.memory = V4L2_MEMORY_MMAP;

if (ioctl(eventDevice, VIDIOC_QUERYBUF, &buf) == 0) { // if request buffer succeded
ALOGI("Buffer offset from VIDIOC_QUERYBUF: 0x%x", buf.m.offset);
}


if (event.addr % getpagesize() != 0) {
ALOGE("event.addr is not page-aligned: 0x%llx", (long long)event.addr);
break;
}
if (fcntl(eventDevice, F_GETFD) == -1){
ALOGI("Invalid File descriptor");

}

void *test_map = mmap(NULL, 4096, PROT_READ | PROT_WRITE, MAP_SHARED, eventDevice, 0);
if (test_map == MAP_FAILED) {
ALOGE("Test mmap failed with fd=%d, errno=%d (%s)", eventDevice, errno, strerror(errno));
} else {
ALOGI("Test mmap succeeded. Address: %p", test_map);
munmap(test_map, 4096);
}

long page_size = getpagesize();
off_t small_offset = page_size; // try offset 4096
size_t small_size = page_size; // 4096 bytes

void* second_test_map = mmap(NULL, small_size, PROT_READ | PROT_WRITE, MAP_SHARED, eventDevice, small_offset);
if (second_test_map == MAP_FAILED) {
ALOGE("Second test mmap failed: fd=%d, offset=0x%llx, errno=%d (%s)",
eventDevice, (long long)small_offset, errno, strerror(errno));
} else {
ALOGI("Second test mmap succeeded. Address: %p (offset=0x%llx)",
second_test_map, (long long)small_offset);
munmap(second_test_map, small_size);
}

}

void *mapped_json_buffer = NULL; // Use a temporary pointer for mmap result

ALOGI("Calling mmap(NULL, %u, PROT_READ|PROT_WRITE, MAP_SHARED, %d, 0x%llx)",
VIV_JSON_BUFFER_SIZE, eventDevice, (long long)event.addr);

// Check if the address is already mapped in bufMap
auto it = bufMap.find(event.addr);
if (it == bufMap.end()) {
ALOGI("VIV_VIDEO_EVENT_EXTCTRL: event.addr not found in bufMap. Attempting mmap...");
// Not found, attempt to mmap
mapped_json_buffer = ::mmap(NULL, VIV_JSON_BUFFER_SIZE,
PROT_READ | PROT_WRITE, MAP_SHARED, eventDevice, event.addr);

if (mapped_json_buffer == MAP_FAILED) {
// CRITICAL ERROR: mmap failed
ALOGE("VIV_VIDEO_EVENT_EXTCTRL: FAILED to mmap memory for event.addr=0x%llx, fd=%d, size=%zu. errno=%d (%s)",
(long long)event.addr, eventDevice, (size_t)VIV_JSON_BUFFER_SIZE, errno, strerror(errno));
}
// mmap successful, store in bufMap
ALOGI("VIV_VIDEO_EVENT_EXTCTRL: mmap successful. Mapped address: 0x%p", mapped_json_buffer);
bufMap[event.addr] = mapped_json_buffer;
} else {
// Already mapped, retrieve from bufMap
ALOGI("VIV_VIDEO_EVENT_EXTCTRL: event.addr found in bufMap. Retrieving mapped address.");
mapped_json_buffer = it->second;
}

ALOGI("VIV_VIDEO_EVENT_EXTCTRL: Mapped buffer pointer: 0x%p", mapped_json_buffer);

// Double-check if the pointer is valid before using it
if (mapped_json_buffer == MAP_FAILED || mapped_json_buffer == NULL) {
ALOGE("VIV_VIDEO_EVENT_EXTCTRL: Mapped buffer is invalid (0x%p) after mmap/lookup. Skipping JSON parsing.", mapped_json_buffer);
}

Json::Reader reader;
// Now, safely use the mapped_json_buffer
std::string str = (char *)mapped_json_buffer; // This line crashes

---
The second test map is failed which makes me think that there is trying to map a empty space.

 

--------
This is my init sequence

cd
cd build-out/sdk
export LD_LIBRARY_PATH=$pwd:$LD_LIBRARY_PATH
export GST_DEBUG=4
systemctl stop imx8-isp.service
export ISP_LOG_LEVEL=8

rmmod vvcam-video
rmmod vvcam-dwe
rmmod vvcam-isp
rmmod imx8-media-dev.ko
insmod mt9v024.ko
insmod vvcam-isp.ko
insmod vvcam-dwe.ko
insmod vvcam-video.ko # this sets the previous drivers as media
insmod imx8-media-dev.ko
./isp_media_server CAMERA0&

and then one previously mentioned commands (gts or v4l2)
---
I have barely change the OS08a20_8M_10_1080p_hdr.xml and sensor_dwe_os08a20_1080P_config.json so i got my custom files, but i think it should be enough to get a image, even if its not good quality, i changed the resolution to 720x480p,
Files overview:

root@imx8mp:~/build-out/sdk# ls
MT9V024_8M_10_480p_linear.xml libadpcc.so libcam_device.so libhal.so libsom_ctrl.so
OS08a20_8M_10_1080p_hdr.xml libadpf.so libcam_engine.so libi2c_drv.so libversion.so
OS08a20_8M_10_1080p_linear.xml libaec.so libcameric_drv.so libibd.so libvom_ctrl.so
OS08a20_8M_10_4k_hdr.xml libaee.so libcameric_reg_drv.so libisi.so libvvdisplay_shared.so
OS08a20_8M_10_4k_linear.xml libaf.so libcim_ctrl.so libjsoncpp.so mt9v024.drv
Sensor0_Entry.cfg libaflt.so libcommon.so libjsoncpp.so.1.9.0 mt9v024.ko
Sensor0_Entry_mt9v024.cfg libahdr.so libcppnetlib-client-connections.so libjsoncpp.so.21 os08a20.drv
Sensor0_Entry_os08a20.cfg libappshell_ebase.so libcppnetlib-client-connections.so.0 libmedia_server.so os08a20.ko
Sensor1_Entry.cfg libappshell_hal.so libcppnetlib-client-connections.so.0.13.0 libmim_ctrl.so ov2775.ko
Sensor1_Entry_mt9v024.cfg libappshell_ibd.so libcppnetlib-server-parsers.so libmipi_drv.so run.sh
Sensor1_Entry_os08a20.cfg libappshell_oslayer.so libcppnetlib-server-parsers.so.0 libmom_ctrl.so start_isp.sh
VSI_Monitor.cfg libavs.so libcppnetlib-server-parsers.so.0.13.0 libmt9v024.so test_image.ogv
basler-camera-driver-vvcam.ko libawb.so libcppnetlib-uri.so libmt9v024.so.1 video_test
dewarp_config libawdr3.so libcppnetlib-uri.so.0 libmt9v024.so.1.0.0 vvcam-dwe.ko
imx8-media-dev.ko libbase64.so libcppnetlib-uri.so.0.13.0 libos08a20.so vvcam-isp.ko
isp_media_server libbufferpool.so libdewarp_hal.so libos08a20.so.1 vvcam-video.ko
liba2dnr.so libbufsync_ctrl.so libebase.so libos08a20.so.1.0.0 vvext
liba3dnr.so libcam_calibdb.so libfpga.so liboslayer.so
\root@imx8mp:~/build-out/sdk# ls dewarp_config/
sensor_dwe_bypass_480P_config.json sensor_dwe_os08a20_1080P_config.json sensor_dwe_os08a20_4K_config.json
root@imx8mp:~/build-out/sdk# cat dewarp_config/sensor_dwe_bypass_480P_config.json
{
"dewarpConfigArray" :[
{
"source_image":{
"width" : 752,
"height" : 480
},

"?dewarpType": "LENS_CORRECTION, FISHEYE_EXPAND, SPLIT_SCREEN",
"dewarpType": "FISHEYE_DEWARP",

"scale": {
"roix" : 0,
"roiy" : 0,
"factor" : 1.0
},

"split": {
"horizon_line" : 240,
"vertical_line_up" : 367,
"vertical_line_down": 367
},

"bypass" : true,
"hflip" : false,
"vflip" : false,

"camera_matrix" : [ 3.9177894938743270e+003, 0., 1.9716642989691159e+003, 0.,3.9177894938743270e+003, 1.1024451486734267e+003, 0., 0., 1. ],
"distortion_coeff": [ -1.3019040624278982e-001, 2.2621318183135611e-001,1.2109476203374344e-003, 9.4317229120640680e-004,-7.1053958306120402e-001 ],
"perspective" : [1.0, 0, 0, 0, 1, 0, 0, 0, 1]

}
]

}
root@imx8mp:~/build-out/sdk# cat Sensor0_Entry.cfg
name="mt9v024"
drv = "mt9v024.drv"
mode= 0

[mode.0]
xml = "MT9V024_8M_10_480p_linear.xml"
dwe = "dewarp_config/sensor_dwe_bypass_480P_config.json"root@imx8mp:~/build-out/sdk#

---
This is how my media looks like (I recalled I tried another isp project and I had media1 as well, but that was in yocto scarthgap, so I dont know if should be the same here):

root@imx8mpmk5:~/build-out/sdk# media-ctl -p -d /dev/media0
Media controller API version 5.15.71

Media device information

driver mxc-md
model FSL Capture Media Device
serial
bus info
hw revision 0x0
driver version 5.15.71

Device topology
- entity 1: mxc-mipi-csi2.0 (8 pads, 1 link)
type Node subtype V4L flags 0
device node name /dev/v4l-subdev2
pad0: Sink
<- "mt9v024 2-0048":0 [ENABLED,IMMUTABLE]
pad1: Sink
pad2: Sink
pad3: Sink
pad4: Source
pad5: Source
pad6: Source
pad7: Source

- entity 10: mt9v024 2-0048 (1 pad, 1 link)
type V4L2 subdev subtype Sensor flags 0
device node name /dev/v4l-subdev3
pad0: Source
[fmt:unknown/0x0]
-> "mxc-mipi-csi2.0":0 [ENABLED,IMMUTABLE]

root@imx8mpm:~/build-out/sdk# media-ctl -p -d /dev/media1
Failed to enumerate /dev/media1 (-2)

----

I hope someone can give me a hint of how to further debug this or point me which component is generating this issue.

标记 (1)
0 项奖励
回复
1 解答
221 次查看
r3gl0
Contributor II
Hey, I think that isp-imx-4.2.2.20.0 does not have the mentioned migration issue.

I fixed it by utilizing:
./build-all-isp.sh release partial V4L2
instead of
./build-all-isp.sh release partial

I was reading a manual from yocto scarthgap which default mode is V4L2, so I was building in native mode instead of V4L2, since in isp-imx-4.2.2.20.0 the default mode is "native sensor".

在原帖中查看解决方案

0 项奖励
回复
2 回复数
248 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello

with the https://docs.nxp.com/bundle/AN13712/page/topics/start_isp_media_server.html

maintain the extracted isp-imx in your repository for customized driver development. However, the diff tool, did not see the difference of .so files during the migration from isp-imx-4.2.2.6.0 to isp-imx-4.2.2.11.0 . Thus, they stayed the same as isp-imx-4.2.2.6.0 and faced the same issue as described in IMX8M-Plus Camera Integration and using ISP.

 

Regards

 

0 项奖励
回复
222 次查看
r3gl0
Contributor II
Hey, I think that isp-imx-4.2.2.20.0 does not have the mentioned migration issue.

I fixed it by utilizing:
./build-all-isp.sh release partial V4L2
instead of
./build-all-isp.sh release partial

I was reading a manual from yocto scarthgap which default mode is V4L2, so I was building in native mode instead of V4L2, since in isp-imx-4.2.2.20.0 the default mode is "native sensor".
0 项奖励
回复