is there still some flash compatible with IMX27 to replace : S34MS01G100BHI000 SPANSION (128Mbytes / 2Kbytes per page / 64 pages per bloc / extra data of 64 bytes per page) which are EOL?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

is there still some flash compatible with IMX27 to replace : S34MS01G100BHI000 SPANSION (128Mbytes / 2Kbytes per page / 64 pages per bloc / extra data of 64 bytes per page) which are EOL?

1,178 次查看
catherinedavid
NXP Employee
NXP Employee
  • New Flash model : S34MS02G204BHI010 SPANSION (256Mbytes / 2Kbytes per page / 64 pages per bloc / extra data of 128 bytes per page)

we have implemented the ATK support for this new flash as described by https://www.nxp.com/docs/en/application-note/AN3985.pdf but the ADS ToolKit (ATK) keeps indicating “Failed to initial flash”.

 

We have performed both hardware and software checks without finding anything wrong, so it could help if :

  •  we are also interested by the software changes (particularly for ATK support (Redboot or Linux)
0 项奖励
回复
2 回复数

1,072 次查看
miduo
NXP Employee
NXP Employee

Hi,

I seems that you put the question in wrong location. Please move this post to I.MX community:https://community.nxp.com/community/imx?tid=community 

Thanks.

0 项奖励
回复

1,073 次查看
TomE
Specialist II

> Please move

Under the "Actions" Menu thing at top-right the Author can see a "Move" option. Use that.

Tom

0 项奖励
回复