Is there a register to set to revert the pixel of lvds0 and lvds?That is when lvds0 output the first pixel and lvds1 output the second pixel,after modifing the register lvds0 output the second pixel and lvds1 output the first pixel,so,such a register exist in Imx6 or not ?
do you mean split channel, right? refer to the Reference Manual, Table Channel Mapping, LVDS Channel 0 get the first pixel from DI0 or DI1, LVDS Channel 1 get the second pixel from DI0 or DI 1, if you need to swap them, I think you need to do it by your own software.