internal storage not mounted after factory reset on i.mx6 platform

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

internal storage not mounted after factory reset on i.mx6 platform

1,695件の閲覧回数
lqw39
Contributor III

Hi, all,

We encountered a critical issue: internal storage cannot be mounted after factory reset.

Internal storage is correct after I download images via MFGTool, and mount info is:

rootfs / rootfs ro,relatime 0 0

tmpfs /dev tmpfs rw,nosuid,relatime,mode=755 0 0

devpts /dev/pts devpts rw,relatime,mode=600 0 0

proc /proc proc rw,relatime 0 0

sysfs /sys sysfs rw,relatime 0 0

none /acct cgroup rw,relatime,cpuacct 0 0

tmpfs /mnt/secure tmpfs rw,relatime,mode=700 0 0

tmpfs /mnt/asec tmpfs rw,relatime,mode=755,gid=1000 0 0

tmpfs /mnt/obb tmpfs rw,relatime,mode=755,gid=1000 0 0

tmpfs /mnt/shm tmpfs rw,relatime,size=1024k,mode=775,uid=1000,gid=1003 0 0

none /dev/cpuctl cgroup rw,relatime,cpu 0 0

/dev/block/mmcblk0p5 /system ext4 ro,relatime,user_xattr,acl,barrier=1,data=ordered 0 0

/dev/block/mmcblk0p4 /data ext4 rw,nosuid,nodev,noatime,nodiratime,errors=panic,user_xattr,acl,barrier=1,nomblk_io_submit,data=ordered,noauto_da_alloc 0 0

/dev/block/mmcblk0p6 /cache ext4 rw,nosuid,nodev,relatime,user_xattr,acl,barrier=1,nomblk_io_submit,data=ordered 0 0

/dev/block/mmcblk0p7 /device ext4 ro,relatime,user_xattr,acl,barrier=1,data=ordered 0 0

/dev/block/mmcblk0p8 /vendor ext4 rw,nosuid,nodev,relatime,user_xattr,acl,barrier=1,data=ordered 0 0

none /sys/kernel/debug debugfs rw,relatime 0 0

/dev/fuse /mnt/shell/emulated fuse rw,nosuid,nodev,relatime,user_id=1023,group_id=1023,default_permissions,allow_other 0 0

/dev/block/vold/179:25 /mnt/extsd vfat rw,dirsync,nosuid,nodev,noexec,relatime,uid=1000,gid=1023,fmask=0002,dmask=0002,allow_utime=0020,codepage=cp437,iocharset=iso8859-1,shortname=mixed,utf8,errors=remount-ro 0 0

But internal storage cannot be mounted after factory reset, the mount info is:

rootfs / rootfs ro,relatime 0 0

tmpfs /dev tmpfs rw,nosuid,relatime,mode=755 0 0

devpts /dev/pts devpts rw,relatime,mode=600 0 0

proc /proc proc rw,relatime 0 0

sysfs /sys sysfs rw,relatime 0 0

none /acct cgroup rw,relatime,cpuacct 0 0

tmpfs /mnt/secure tmpfs rw,relatime,mode=700 0 0

tmpfs /mnt/asec tmpfs rw,relatime,mode=755,gid=1000 0 0

tmpfs /mnt/obb tmpfs rw,relatime,mode=755,gid=1000 0 0

tmpfs /mnt/shm tmpfs rw,relatime,size=1024k,mode=775,uid=1000,gid=1003 0 0

none /dev/cpuctl cgroup rw,relatime,cpu 0 0

/dev/block/mmcblk0p5 /system ext4 ro,relatime,user_xattr,acl,barrier=1,data=ordered 0 0

/dev/block/mmcblk0p4 /data ext4 rw,nosuid,nodev,noatime,nodiratime,errors=panic,user_xattr,acl,barrier=1,nomblk_io_submit,data=ordered,noauto_da_alloc 0 0

/dev/block/mmcblk0p6 /cache ext4 rw,nosuid,nodev,relatime,user_xattr,acl,barrier=1,nomblk_io_submit,data=ordered 0 0

/dev/block/mmcblk0p7 /device ext4 ro,nosuid,nodev,relatime,user_xattr,acl,barrier=1,data=ordered 0 0

none /sys/kernel/debug debugfs rw,relatime 0 0

/dev/block/vold/179:25 /mnt/extsd vfat rw,dirsync,nosuid,nodev,noexec,relatime,uid=1000,gid=1023,fmask=0002,dmask=0002,allow_utime=0020,codepage=cp437,iocharset=iso8859-1,shortname=mixed,utf8,errors=remount-ro 0 0

There is no /dev/fuse.

Anyone can help me?

Thanks.

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,246件の閲覧回数
YixingKong
Senior Contributor IV

Qingwei

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 件の賞賛
返信

1,246件の閲覧回数
YixingKong
Senior Contributor IV

Qingwei

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,
Yixing

0 件の賞賛
返信

1,246件の閲覧回数
raymondwang
Senior Contributor I

You'd better paste your logcat log to capture error.

0 件の賞賛
返信