installing vivante X11 library files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

installing vivante X11 library files

2,197 Views
srinivasaporam
Contributor II

Hi,

We are facing problem with X in our ubuntu which is been ported to imx6Q board.

We came to know that for X with vivante we need to install following:

xserver-xorg-video-imx-viv-5.0.11.p7.1

So, We have got xserver-xorg-video-imx-viv-5.0.11.p7.1.tar.gz.

Can anybody please explain me how to build these and deploy to the target machine.

We already cross-compiled 3.10.53 or 3.14.14 and board is booting to ubuntu14.04. Now we have got

1.kernel-module-imx-gpu-viv-5.0.11.p7.1.tar.gz

2. xserver-xorg-video-imx-viv-5.0.11.p7.1.tar.gz

is there any document that explains installing above ?????

Labels (3)
0 Kudos
Reply
1 Reply

1,357 Views
igorpadykov
NXP Employee
NXP Employee

Hi Srinivasa

NXP/FSL BSPs do not support ubuntu,

for integration ubunty trusty with vivante drivers one can look at

https://boundarydevices.com/ubuntu-trusty-for-i-mx6-boards-june-2015-kernel-3-10-53/

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply