when installing opencv on imx6 board using bitbake command
I get opencv_3.1 installed
$ bitbake -s | grep opencv
opencv :3.1+gitAUTOINC+92387b1ef8-r0
which file should i edit to install opencv_2.4.8 on imx6 board
Hi Sheraz,
First pls check if your bsp has opencv2.4 or not, if yes, pls try to set PREFERRED_VERSION_opencv to 2.4 if not you have to install yocto 3.10.52.
Regards
Hi Bio_TICFSL
In opencv_2.4.bb i commenented the following line
#PNBLACKLIST[opencv] ?= "Not compatible with currently used ffmpeg 3"
and set PREFERRED_VERSION_opencv to 2.4 but one opencv library is missing
libopencv_ts.so.2.4
Regrds