install gcc and toolchain on target rfs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

install gcc and toolchain on target rfs

1,822 Views
sabeel_syed
NXP Employee
NXP Employee

Please help to get a reciepe to install tool chain on target.

This would let compile on the target platform.

please let us know any suggession on how to do it.

0 Kudos
Reply
1 Reply

1,429 Views
b36401
NXP Employee
NXP Employee

You can include such lines

IMAGE_FEATURES += " \
dev-pkgs \
tools-sdk \
"

into local.conf file to add gcc compiler into building image.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply