inline ECC in i.MX8M Plus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

inline ECC in i.MX8M Plus

跳至解决方案
4,468 次查看
anhui527
Contributor III
Hi, NXP experts are there any documents about the function of inline ECC in i.MX8M plus ? thanks.
0 项奖励
回复
1 解答
4,465 次查看
joanxie
NXP TechSupport
NXP TechSupport

don't find any document for this, but get the information from expert team:
"The 8M Plus will support the DRAM inline ECC feature, however, it is currently being validated. Once validation is complete further information on the support will be made available.

This is an optional feature and customers will be allowed to enable or disable as well as configure the regions they want to be ECC protected. When enabled there will be a portion of DRAM (up to 1/8th the total density) that will have to be reserved. Also, there are performance and boot time implications with the feature enabled. For Inline ECC, 64/8 SECDED Hamming code is used and Data to ECC ratio is 8/1"

在原帖中查看解决方案

3 回复数
2,148 次查看
bernhardfink
NXP Employee
NXP Employee

Inline ECC in i.MX 8M Plus can be enabled (and tested) using the DDR Configuration tool in the i.MX Config Tool.

https://www.nxp.com/design/design-center/development-boards-and-designs/i-mx-evaluation-and-developm...

 

0 项奖励
回复
3,944 次查看
Anishamd
Contributor I

how do we enable ECC in i.MX8M Plus can you share any documents if you have.

0 项奖励
回复
4,466 次查看
joanxie
NXP TechSupport
NXP TechSupport

don't find any document for this, but get the information from expert team:
"The 8M Plus will support the DRAM inline ECC feature, however, it is currently being validated. Once validation is complete further information on the support will be made available.

This is an optional feature and customers will be allowed to enable or disable as well as configure the regions they want to be ECC protected. When enabled there will be a portion of DRAM (up to 1/8th the total density) that will have to be reserved. Also, there are performance and boot time implications with the feature enabled. For Inline ECC, 64/8 SECDED Hamming code is used and Data to ECC ratio is 8/1"