initialization code of Enhanced SDRAM Controller (i.MX51 WEC7)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

initialization code of Enhanced SDRAM Controller (i.MX51 WEC7)

844件の閲覧回数
eishishibusawa
Contributor III

Dear Sir

 

I want to ask about initialization code of Enhanced SDRAM Controller (eSDCTL).

I cannot find the init code in WEC7 BSP for i.MX51.

Which source file of i.MX51 WEC7 BSP contains the init code?

 

Best Regards,

Eishi SHIBUSAWA

 

ラベル(2)
0 件の賞賛
返信
1 返信

747件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

please check

WEC7/PLATFORM/iMX51_EVK/SRC/BOOTLOADER/EBOOT/flash_header.s

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信