Hi,
I connected FPGA to i.mx6q on pcie bus and need to access over 128MB memory area.
I found that it seems to be a limit of 15MB for PCIE assigned memory regions under which everything's ok
and over which I get these messages on kernel startup.
PCI host bridge to bus 0000:00
pci_bus 0000:00: root bus resource [io 0x1000-0x10000]
pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]
pci_bus 0000:00: No busn resource found for root bus, will use [bus 00-ff]
PCI: bus0: Fast back to back transfers disabled
PCI: bus1: Fast back to back transfers disabled
pci 0000:01:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
PCI: bus2: Fast back to back transfers enabled
pci 0000:00:00.0: BAR 8: can't assign mem (size 0xa000000)
pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]
pci 0000:00:00.0: BAR 9: assigned [mem 0x01100000-0x011fffff pref]
pci 0000:00:00.0: BAR 6: assigned [mem 0x01200000-0x0120ffff pref]
pci 0000:00:00.0: BAR 7: assigned [io 0x1000-0x1fff]
pci 0000:01:00.0: BAR 8: can't assign mem (size 0xa000000)
pci 0000:01:00.0: BAR 0: assigned [mem 0x01100000-0x0110ffff 64bit pref]
pci 0000:01:00.0: BAR 7: assigned [io 0x1000-0x1fff]
pci 0000:02:04.0: BAR 2: can't assign mem (size 0x4000000)
pci 0000:02:04.0: BAR 3: can't assign mem (size 0x4000000)
pci 0000:02:04.0: BAR 0: can't assign mem (size 0x200)
pci 0000:02:04.0: BAR 1: assigned [io 0x1000-0x10ff]
pci 0000:01:00.0: PCI bridge to [bus 02]i
pci 0000:01:00.0: bridge window [io 0x1000-0x1fff]
pci 0000:00:00.0: PCI bridge to [bus 01-02]
pci 0000:00:00.0: bridge window [io 0x1000-0x1fff]
pci 0000:00:00.0: bridge window [mem 0x01100000-0x011fffff pref]
PCI: enabling device 0000:01:00.0 (0140 -> 0143)
I use Inbound PCIE which can access 4GB external memory area in term of
[i.MX 6 Dual/6Quad Applicatiuons Processor Reference Manual].
In default it can access inbound PCIE 15MB memory area in test of result and above document.
I want to know if it possible to access inbound PCIE 129MB memory area by modify source code or other methods.
Can someone help me to find a solution?
Thank you very much.
David