use imxrt1170-evk
1. I want to use jtag to load only .axf files.
i try MCUBOOTUtility and Secure Provisioning Tool.
But, tools doesn't seem to have jtag loading.
When I used that tool to load to USB, I succeeded.
so how can i slove this problem?
2. An error is generated when trying several times program build situation
region `SRAM_DTC_cm7' overflowed by 165744 bytes
Memory region Used Size Region Size %age Used
BOARD_FLASH: 0 GB 16 MB 0.00%
SRAM_DTC_cm7: 427888 B 256 KB 163.23%
SRAM_ITC_cm7: 0 GB 256 KB 0.00%
SRAM_OC1: 0 GB 512 KB 0.00%
...
make[1]: *** [makefile:69: TEST.axf] Error 1
make: *** [makefile:60: all] Error 2
What needs to be fixed???
Solved! Go to Solution.
Hello, thanks for your information, I found this thread Using J-Link with MIMXRT1160-EVK or MIMXRT1170-EVK - NXP Community please follow the instructions.
Then download the J-Link Commander. [J-Link Commander (segger.com)] and follow this command.
connect
?
Then this popup window appears to select your target device RT1176xxx [example image].
In the next options click enter, which will be for interface and speed.
If all is right, you cand try the next command to upload the .bin as a test communication.
loadfile C:\Debugin\example.bin
You need to replace the root.
Best regards,
Pavel
Hello, my name is Pavel, and I will be supporting your case, I review your information and I did a test.
The .axf is supported by the tool.
Let me know if the issue persists and elaborate further about your issue.
Best regards,
Pavel
I want to turn on the power without connecting J11 (usb) and insert the firmware using only the JTAG (J1) part.
Hello, are you using the EVK? if yes maybe the MIMXRT1170 EVK Board Hardware User’s Guide could help you, please review chapter 2.12, then could you upload an image about your setup? and tell me, what kind of debugger you are using?
Best regards,
Pavel
hello,
i review chapter 2.12, remove R187, R208, R195 and R78 is right?
i try this setting, and J38(1-2), SW1(10-Internal BOOT)
An error occurs when trying to debug as segger with the MCUXpressoIDE also...
I use J-Link Base Segger debugger.
For reference, I am using the IMXRT1170-EVK-PXP example linked with Embedded Wizard.
GPIO_LPSR_13(JTAG_MOD) is need to pull-up??
Hello, thanks for being clear, I review your information seems good, you mentioned you are using the J-Link and the image was for LPCLinkServer, could you share an image about your setup? to review how you are connected between the RT and the debug probe.
Best regards,
Pavel
mimxrt-1170-evk
-> i remove R187, R208, R195, R78
shut down error image
JLink debug configuration
Hello, thanks for your information, I found this thread Using J-Link with MIMXRT1160-EVK or MIMXRT1170-EVK - NXP Community please follow the instructions.
Then download the J-Link Commander. [J-Link Commander (segger.com)] and follow this command.
connect
?
Then this popup window appears to select your target device RT1176xxx [example image].
In the next options click enter, which will be for interface and speed.
If all is right, you cand try the next command to upload the .bin as a test communication.
loadfile C:\Debugin\example.bin
You need to replace the root.
Best regards,
Pavel
thanks i didn't think of that
i have a problem...
target interface : swd
other option is default mode
after loadfile , firmware not change..
Is there anything else I need to do, such as verify?
Hello, in the menu appears 3 options JTAG, SWD and etc. you must select the JTAG option.
Best regards,
Pavel