Please, advise a sample project to read/write/erase with QSPI memory provided on imxrt1020_evk.
Thank you in advance.
Best regards,
Oleksii
Hi Oleksii,
Please refer to the flexspi_nor_polling_transfer example of the SDK. In this example, flexspi will send data and operate the external Nor flash connected with FLEXSPI. Some simple flash command will be executed, such as Write Enable, Erase sector, Program page.
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------