Re: imxrt1010 SAI_TransferSendEDMA / SAI_TransferReceiveEDMA can't be used for ping-pong buffers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: imxrt1010 SAI_TransferSendEDMA / SAI_TransferReceiveEDMA can't be used for ping-pong buffers

1,685 Views
bowerymarc
Contributor V

Hi Jeremy,

You need to try to build one of those demos using the code generated by the configuration tool.  Walk through it as I have.  You will find that the code pulled in by the config tool preclude the uses you claim they can.  You are clearly unfamiliar with the config tool code.

If the configuration tool is not able to provide for these common scenarios, your team needs to revise the tool, not tell your customers that it's useless. 

The older Kinetis tools were much more useful.  As are the ST Micro CubeMX.  NXP needs to step up it's game.

Best,

Marc

0 Kudos
Reply
2 Replies

1,501 Views
jeremyzhou
NXP Employee
NXP Employee

Hi
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I'll give it a try, and you'd better describe what exactly demo you want to create and demonstrate the steps of configuring the config tool you did.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,435 Views
bowerymarc
Contributor V

you can try the sai demo app, or one of the USB audio apps.  They all have the same underlying driver code. 

thx

M

0 Kudos
Reply