imxg2dvideosink does not work in Igor's image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imxg2dvideosink does not work in Igor's image

851件の閲覧回数
elshadmustafaye
Contributor I

Hi everyone.

I am using Igor's Debian Jessie for hummingboard IMX6. I compiled version 0.12.0 of https://github.com/Freescale/gstreamer-imxand installed it. I can use imxipuvideosink just fine. However, I can't get imxg2dvideosink working.

When I try the following pipeline:

gst-launch-1.0 videotestsrc ! imxg2dvideosink

I get

$ sudo gst-launch-1.0 videotestsrc ! imxg2dvideosink

Setting pipeline to PAUSED ...

Pipeline is PREROLLING ...

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922228] Internal error: Oops: 5 [#4] SMP ARM

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922381] Process videotestsrc0:s (pid: 2506, stack limit = 0xad26a238)

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922387] Stack: (0xad26bd68 to 0xad26c000)

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922397] bd60: 00000000 00000000 00000001 800fe7a0 ffffffff 00000000

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922406] bd80: 00000000 00000000 00000000 00000000 000009c9 00000000 0000000e ad174d88

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922416] bda0: 00000000 ad26be60 ad26be20 800bbf00 00000001 800f69fc ac9cb180 ac396c00

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922425] bdc0: ad07f000 ad26a020 00007530 ad26a000 00000006 ac0d04d8 6e42b3f0 804e4b7c

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922435] bde0: 6e42b438 00000000 000000f8 00000000 6e42b438 00000000 000000f8 00000000

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922444] be00: 00000023 00000002 6e42b840 00000001 76f63000 01d7a550 00000002 00000001

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922453] be20: 00000001 76ee5021 01d6f2f0 76f63000 80000000 00000000 7688363f 00000000

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922463] be40: 6dc00000 0001c200 6e42b840 00000002 6e42b840 76ee5235 76e53c88 add7c100

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922472] be60: 76992d44 01d87730 76f63000 6e42b840 01d87730 76f63000 6e42b840 00000001

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922481] be80: 00000000 76ec43f9 000000f0 00000003 6db2c0fc 6db2c10c 00000000 00000000

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922491] bea0: 76f63000 01d6f568 00026230 76f64430 6e42b530 00000002 76990000 00017700

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922500] bec0: 00000002 6db01424 6e42b840 6e42b7d0 01d87730 76963121 00000002 6e42b538

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922510] bee0: 6e42b5d4 00000000 76f64218 76ec5ce5 00026230 6e42b7a0 ad094601 ad094600

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922519] bf00: 6e42b3f0 00007530 00000000 00000006 ac0d04d8 80115a90 aaa2b990 ad174ca8

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922529] bf20: 80a3b188 00000000 ad174ca8 00000000 ac07bb50 76992d44 7fffffff 76dd019d

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922538] bf40: 000000f0 00000001 00000000 00000001 76e53ca0 80084cf8 76992d44 00000000

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922547] bf60: ffffffff ad094601 ad094600 6e42b3f0 00007530 00000000 00000006 00000000

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922557] bf80: 7694f630 80115cbc 01d78420 00002710 76788e80 00007530 00000036 8000e224

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922566] bfa0: ad26a000 8000e0a0 00002710 76788e80 00000006 00007530 6e42b3f0 01d78420

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922576] bfc0: 00002710 76788e80 00007530 00000036 000000f8 6e42b748 76f64430 7694f630

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922585] bfe0: 76785100 6e42b3dc 7676aab0 76cfa206 200f0030 00000006 3ff7e821 3ff7ec21

Message from syslogd@localhost at Jun 1 15:40:46 ...

kernel:[ 1815.922664] Code: e3042d56 e3442d45 e598c030 e598e038 (e5911000)

After it just hangs. The same pipeline works fine in Solidrun's debian jessie image. I am looking for suggestions on how to fix this issue.

I don't know what information to paste here. Here is the output of uname -a

$ uname -a

Linux cubox-i 3.14.67-cubox #2 SMP Fri Apr 29 03:34:19 CEST 2016 armv7l GNU/Linux

The dmesg output when the pipeline runs is:

[ 1815.922228] Internal error: Oops: 5 [#4] SMP ARM

[ 1815.922234] Modules linked in: xt_multiport nf_conntrack_ipv4 nf_defrag_ipv4 xt_conntrack nf_conntrack cpufreq_stats bluetooth 6lowpan_iphc arc4 iwldvm mac80211 iwlwifi cfg80211 rfkill ir_lirc_codec ir_mce_kbd_decoder lirc_dev ir_sanyo_decoder ir_sony_decoder ir_rc6_decoder ir_rc5_decoder ir_nec_decoder ir_jvc_decoder gpio_ir_recv bonding

[ 1815.922295] CPU: 1 PID: 2506 Comm: videotestsrc0:s Tainted: G D 3.14.67-cubox #2

[ 1815.922304] task: aca88b00 ti: ad26a000 task.ti: ad26a000

[ 1815.922319] PC is at gckKERNEL_Dispatch+0x568/0x1488

[ 1815.922330] LR is at 0x7688363f

[ 1815.922339] pc : [<804ebe90>] lr : [<7688363f>] psr: 200f0013

sp : ad26bd68 ip : 80000000 fp : 6e42b3f0

[ 1815.922347] r10: ac0d04d8 r9 : ac37e700 r8 : ad26be00

[ 1815.922353] r7 : 00000000 r6 : ad26a020 r5 : 00000001 r4 : 00000000

[ 1815.922359] r3 : 6dc00000 r2 : 4d454d56 r1 : ebebebeb r0 : 00000000

[ 1815.922367] Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user

[ 1815.922374] Control: 10c53c7d Table: 3d25804a DAC: 00000015

[ 1815.922381] Process videotestsrc0:s (pid: 2506, stack limit = 0xad26a238)

[ 1815.922387] Stack: (0xad26bd68 to 0xad26c000)

[ 1815.922397] bd60: 00000000 00000000 00000001 800fe7a0 ffffffff 00000000

[ 1815.922406] bd80: 00000000 00000000 00000000 00000000 000009c9 00000000 0000000e ad174d88

[ 1815.922416] bda0: 00000000 ad26be60 ad26be20 800bbf00 00000001 800f69fc ac9cb180 ac396c00

[ 1815.922425] bdc0: ad07f000 ad26a020 00007530 ad26a000 00000006 ac0d04d8 6e42b3f0 804e4b7c

[ 1815.922435] bde0: 6e42b438 00000000 000000f8 00000000 6e42b438 00000000 000000f8 00000000

[ 1815.922444] be00: 00000023 00000002 6e42b840 00000001 76f63000 01d7a550 00000002 00000001

[ 1815.922453] be20: 00000001 76ee5021 01d6f2f0 76f63000 80000000 00000000 7688363f 00000000

[ 1815.922463] be40: 6dc00000 0001c200 6e42b840 00000002 6e42b840 76ee5235 76e53c88 add7c100

[ 1815.922472] be60: 76992d44 01d87730 76f63000 6e42b840 01d87730 76f63000 6e42b840 00000001

[ 1815.922481] be80: 00000000 76ec43f9 000000f0 00000003 6db2c0fc 6db2c10c 00000000 00000000

[ 1815.922491] bea0: 76f63000 01d6f568 00026230 76f64430 6e42b530 00000002 76990000 00017700

[ 1815.922500] bec0: 00000002 6db01424 6e42b840 6e42b7d0 01d87730 76963121 00000002 6e42b538

[ 1815.922510] bee0: 6e42b5d4 00000000 76f64218 76ec5ce5 00026230 6e42b7a0 ad094601 ad094600

[ 1815.922519] bf00: 6e42b3f0 00007530 00000000 00000006 ac0d04d8 80115a90 aaa2b990 ad174ca8

[ 1815.922529] bf20: 80a3b188 00000000 ad174ca8 00000000 ac07bb50 76992d44 7fffffff 76dd019d

[ 1815.922538] bf40: 000000f0 00000001 00000000 00000001 76e53ca0 80084cf8 76992d44 00000000

[ 1815.922547] bf60: ffffffff ad094601 ad094600 6e42b3f0 00007530 00000000 00000006 00000000

[ 1815.922557] bf80: 7694f630 80115cbc 01d78420 00002710 76788e80 00007530 00000036 8000e224

[ 1815.922566] bfa0: ad26a000 8000e0a0 00002710 76788e80 00000006 00007530 6e42b3f0 01d78420

[ 1815.922576] bfc0: 00002710 76788e80 00007530 00000036 000000f8 6e42b748 76f64430 7694f630

[ 1815.922585] bfe0: 76785100 6e42b3dc 7676aab0 76cfa206 200f0030 00000006 3ff7e821 3ff7ec21

[ 1815.922606] [<804ebe90>] (gckKERNEL_Dispatch) from [<804e4b7c>] (drv_ioctl+0x120/0x28c)

[ 1815.922623] [<804e4b7c>] (drv_ioctl) from [<80115a90>] (do_vfs_ioctl+0x3fc/0x5bc)

[ 1815.922636] [<80115a90>] (do_vfs_ioctl) from [<80115cbc>] (SyS_ioctl+0x6c/0x7c)

[ 1815.922653] [<80115cbc>] (SyS_ioctl) from [<8000e0a0>] (ret_fast_syscall+0x0/0x38)

[ 1815.922664] Code: e3042d56 e3442d45 e598c030 e598e038 (e5911000)

[ 1815.922674] ---[ end trace 282cadbe45798cf3 ]---

Thanks.

ラベル(1)
0 件の賞賛
返信
0 返答(返信)