imxRT1176 ,erase norflash and IRQ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imxRT1176 ,erase norflash and IRQ

357 Views
xiaozezitian
Contributor I

when we use imxRT1176 MCU.When both cores are used, M7 is used as the main core, M4 is used as the slave core, and M4 uses flexspi to erase and write to the norflash. At this time, do we need to close all interrupts on both cores.

0 Kudos
2 Replies

311 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @xiaozezitian,

I believe this is a duplicated post from the following: https://community.nxp.com/t5/i-MX-Processors/imxRT1176-if-flash-is-to-be-erased-all-interrupts-of-bo...

If it is ok with you, I will provide follow-up on the linked community post in order to prevent double efforts.

BR,
Edwin.

286 Views
xiaozezitian
Contributor I

If flexspi is initialized in the M7 core and then deinit flexspi ,Not using the flexspi interface in M7 anymore。

Then start the M4 core, flexspi is reinitialized in the M4 core,Use the flexspi interface to operate FLASH in M4.

Is it possible to use like this.

0 Kudos