[imx95]display over usb-c hub with hdmi port

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[imx95]display over usb-c hub with hdmi port

844件の閲覧回数
Ahelion
Contributor IV

Hello all,

I have a toradex verdin board with imx95, which has a USB-OTG connector. Is there a way to connect a usb-c hub to it so that I can connect a monitor to the hubs hdmi port?

If yes, can somebody guide me in the right direction on how to accomplish something like this.

Br,

タグ(2)
0 件の賞賛
返信
1 返信

829件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

According to the current datasheet for the i.MX95, it supports USB 3.0.

Setting up the USB version limitation, this specific functionality is not available as part of the Yocto Project for the i.MX processors.

Best regards.

0 件の賞賛
返信