imx95 configured camera (gc05a2)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx95 configured camera (gc05a2)

251件の閲覧回数
yxjiang
Contributor I

HI NXP

1. Download link for camera setup documentation

2. Where is the issue in the log below?

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

226件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @yxjiang 

 

I would suggest you refer to UG10215:  i.MX Camera Porting Guide.

https://www.nxp.com.cn/docs/en/user-guide/UG10215.pdf

This document provides an overview of the i..MX95 applications processor hardware camera subsystem, and then describes its corresponding software architecture with the Linux Kernel and User space.  It also describes the porting instructions and how to configure the 3A algorithms.

 

Regards

Daniel

 

 

 

 

Regards

Daniel

0 件の賞賛
返信

218件の閲覧回数
yxjiang
Contributor I

Why is there an error in the log?
0 件の賞賛
返信

147件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

From the log file, the GC05A2 sensor at I2C address 1-0037 is detected and linked to the CSI interface.

gc05a2 1-0037 → csidev-4ad30000.csi → crossbar → mxc_isi.2 → /dev/video2

 

The format negotiation shows

    • GC05A2 outputs SGRBG10_1X10/2592x1944
    • CSI and ISI are configured for UYVY8_1X16/1920x1080

This implies that format conversion is happening, likely via ISI, and the pipeline is correctly routed to /dev/video2.

Below fail log shows the requested format is not supported by the V4L2 device /dev/ivdeo2

danielchen_0-1759210168607.png

 

 

0 件の賞賛
返信

142件の閲覧回数
yxjiang
Contributor I

HI @danielchen 

     1.Check the formats supported by /dev/video2, in case they do not meet expectations

     2.The format is incorrect; it is suspected that the CSI and the camera are not compatible.

yxjiang_0-1759211343430.png

0 件の賞賛
返信

129件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

which BSP version you are using?  can you try the latest BSP version 6.12.34

0 件の賞賛
返信

126件の閲覧回数
yxjiang
Contributor I

HI @danielchen 

       1.BSP:imx-6.12.20-2.0.0.xml

       2.This version is already very new. Is it necessary to use version 6.12.34?

 

 

 

0 件の賞賛
返信