imx95 configured camera (gc05a2)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx95 configured camera (gc05a2)

275 Views
yxjiang
Contributor I

HI NXP

1. Download link for camera setup documentation

2. Where is the issue in the log below?

Labels (1)
0 Kudos
Reply
6 Replies

250 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @yxjiang 

 

I would suggest you refer to UG10215:  i.MX Camera Porting Guide.

https://www.nxp.com.cn/docs/en/user-guide/UG10215.pdf

This document provides an overview of the i..MX95 applications processor hardware camera subsystem, and then describes its corresponding software architecture with the Linux Kernel and User space.  It also describes the porting instructions and how to configure the 3A algorithms.

 

Regards

Daniel

 

 

 

 

Regards

Daniel

0 Kudos
Reply

242 Views
yxjiang
Contributor I

Why is there an error in the log?
0 Kudos
Reply

171 Views
danielchen
NXP TechSupport
NXP TechSupport

From the log file, the GC05A2 sensor at I2C address 1-0037 is detected and linked to the CSI interface.

gc05a2 1-0037 → csidev-4ad30000.csi → crossbar → mxc_isi.2 → /dev/video2

 

The format negotiation shows

    • GC05A2 outputs SGRBG10_1X10/2592x1944
    • CSI and ISI are configured for UYVY8_1X16/1920x1080

This implies that format conversion is happening, likely via ISI, and the pipeline is correctly routed to /dev/video2.

Below fail log shows the requested format is not supported by the V4L2 device /dev/ivdeo2

danielchen_0-1759210168607.png

 

 

0 Kudos
Reply

166 Views
yxjiang
Contributor I

HI @danielchen 

     1.Check the formats supported by /dev/video2, in case they do not meet expectations

     2.The format is incorrect; it is suspected that the CSI and the camera are not compatible.

yxjiang_0-1759211343430.png

0 Kudos
Reply

153 Views
danielchen
NXP TechSupport
NXP TechSupport

which BSP version you are using?  can you try the latest BSP version 6.12.34

0 Kudos
Reply

150 Views
yxjiang
Contributor I

HI @danielchen 

       1.BSP:imx-6.12.20-2.0.0.xml

       2.This version is already very new. Is it necessary to use version 6.12.34?

 

 

 

0 Kudos
Reply