imx93 yocto build guide with custom hardware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx93 yocto build guide with custom hardware

Jump to solution
1,125 Views
TomC818
Contributor III

Hello! I am currently designing a custom piece of hardware based on imx93 processor. I have built an image following the steps in application note UG10164 and managed to run the image successfully on an imx93 evk.
I am pretty much new to developing linux and any help would be very welcomed; Is there any application note or guide on how to build with yocto for customized hardware and integration of the settings of ddr and pins from the config tool for imx processor?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1 Reply
1,092 Views
pengyong_zhang
NXP Employee
NXP Employee
0 Kudos
Reply