imx93 wrong clock frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx93 wrong clock frequency

跳至解决方案
946 次查看
spawn
Contributor III

Hello,

on an imx93 processor, I configured a clock in the device tree with: 

 

&flexio2 {                                                                                                                                                                                                         
  assigned-clocks = <&clk IMX93_CLK_FLEXIO2>;                                                                                                                                                                      
  assigned-clock-parents = <&clk IMX93_CLK_SYS_PLL_PFD1_DIV2>;                                                                                                                                                     
  assigned-clock-rates = <80000000>;                                                                                                                                                                              
  status = "okay";                                                                                                                                                                                                
                                                                                                                                                                                                                   
  xx {                                                                                                                                                                                                        
    compatible = "xx,xx";                                                                                                                                                                        
    pinctrl-0 = <&pinctrl_xx>;                                                                                                                                                               
    pinctrl-names = "default";                                                                                                                                                                                     
    clocks = <&clk IMX93_CLK_CCM_CKO1>;                                                                                                                                                                            
    assigned-clocks = <&clk IMX93_CLK_CCM_CKO1>;                                                                                                                                                                   
    assigned-clock-rates = <50000000>;                                                                                                                                                                
  };                                                                                                                                                                                                               
};    

 

Then I confirmed that the clock freq is configured to be 50 MHz from the driver with a call to clk_get_rate().

But the signal frequency I measure is in fact 10 MHz.

Do you know what could cause the issue ?

Best Regards

0 项奖励
回复
1 解答
923 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The following resource shows how to change DRAM frequency.

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-8M-Mini-Register-Programming-Aid-DRA...

 

It is for Mx8MM but it works on Mx93. clocks are described in sect. Clock Control Module (CCM) Chapter 30 i.mx93 reference manual

in uboot sources one can look at

imx-common\arm\arch - uboot-imx - i.MX U-Boot 

in linux one needs to follow clock framework rules:
https://www.kernel.org/doc/Documentation/clk.txt 
https://elinux.org/images/b/b8/Elc2013_Clement.pdf 

 

Regards

在原帖中查看解决方案

0 项奖励
回复
1 回复
924 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

The following resource shows how to change DRAM frequency.

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-8M-Mini-Register-Programming-Aid-DRA...

 

It is for Mx8MM but it works on Mx93. clocks are described in sect. Clock Control Module (CCM) Chapter 30 i.mx93 reference manual

in uboot sources one can look at

imx-common\arm\arch - uboot-imx - i.MX U-Boot 

in linux one needs to follow clock framework rules:
https://www.kernel.org/doc/Documentation/clk.txt 
https://elinux.org/images/b/b8/Elc2013_Clement.pdf 

 

Regards

0 项奖励
回复