imx93 lvds panel failed to create device link

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx93 lvds panel failed to create device link

2,638件の閲覧回数
bora
Contributor II

Hi everyone,

I'm working on enabling an LVDS panel on the i.MX93 custom board using Yocto and a custom device tree setup. I'm facing several issues during boot related to the display subsystem and LVDS panel connection. The config file I attached.

Any help or insights would be appreciated!

Thanks in advance!

here is the part of the lvds-panel dts configuration:

/ {
   
lvds_backlight: lvds_backlight {
compatible = "pwm-backlight";
pwms = <&tpm5 2 100000 0>;
//enable-gpios = <&adp5585gpio 8 GPIO_ACTIVE_HIGH>;
//power-supply = <&reg_vdd_12v>;
status = "okay";
 
brightness-levels = < 0  1  2  3  4  5  6  7  8  9
     10 11 12 13 14 15 16 17 18 19
     20 21 22 23 24 25 26 27 28 29
     30 31 32 33 34 35 36 37 38 39
     40 41 42 43 44 45 46 47 48 49
     50 51 52 53 54 55 56 57 58 59
     60 61 62 63 64 65 66 67 68 69
     70 71 72 73 74 75 76 77 78 79
     80 81 82 83 84 85 86 87 88 89
     90 91 92 93 94 95 96 97 98 99
    100>;
default-brightness-level = <80>;
 
};
 
lvds_panel {
 
        compatible = "panel-lvds";
        backlight = <&lvds_backlight>;
    data-mapping = "vesa-24";
        width-mm = <70>;
        height-mm = <52>;
        status = "okay";
port {
panel_lvds_in: endpoint {
remote-endpoint = <&lvds_out>;
};
};
 
        timing {
        clock-frequency = <6500000>;
                    hactive = <320>;
                    vactive = <240>;
                    hsync-len = <1>;
                    hfront-porch = <17>;
                    hback-porch  = <70>;
                    vsync-len    = <1>;
                    vfront-porch = <9>;
                    vback-porch  = <13>;
                    hsync-active = <0>;
                    vsync-active = <0>;
        };
};
};
 
 
&dphy {
status = "disabled";
};
 
&dsi {
status = "disabled";
};
 
&lcdif {
    status = "okay";
assigned-clock-rates = <445333333>, <6500000>, <400000000>, <133333333>;
};
 
&ldb {
status = "okay";
 
lvds-channel@0 {
status = "okay";
 
port@1 {
reg = <1>;
 
lvds_out: endpoint {
remote-endpoint = <&panel_lvds_in>;
};
};
};
};
 
&ldb_phy {
status = "okay";
};

 

These are the relevant boot log messages:

[ 0.348510] platform lvds_panel: Fixed dependency cycle(s) with /ldb-display-controller/lvds-channel@0
[ 0.877239] imx93-ldb ldb-display-controller: Failed to create device link (0x180) with 4ae30000.lcd-controller
[ 1.611948] imx93-ldb ldb-display-controller: Failed to create device link (0x180) with ldb-phy
[ 1.623932] panel-lvds lvds_panel: /lvds_panel: problems parsing panel-timing (-2)
[ 1.631550] panel-lvds: probe of lvds_panel failed with error -2

I also see repeated binding of imx-lcdifv3-crtc.0:

[ 0.868877] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
...
[ 19.317586] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 19.341381] imx-drm display-subsystem: bound imx-lcdifv3-crtc.0 (ops lcdifv3_crtc_ops)
[ 19.427728] platform imx-lcdifv3-crtc.0: deferred probe pending

 

ラベル(3)
タグ(1)
0 件の賞賛
返信
13 返答(返信)

2,108件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @bora 

 

Please use belwo setting whcih i have verified the generation of pixel clock

&lcdif {
	assigned-clock-rates = <45500000>, <6500000>, <400000000>, <133333333>;
};

New PLL:

 

PLL_FRACN_GP(45500000U, 15, 1, 6, 1, 8),




Best Regards,
Zhiming

0 件の賞賛
返信

2,039件の閲覧回数
bora
Contributor II
I tried and still doesnt work, but I tried on imx93 EVK on that it worked actually.I saw screen on the display.
0 件の賞賛
返信

2,142件の閲覧回数
bora
Contributor II

Hi,

I set it 6.5 MHz again and still doesnt work I see /dev/fb0. I attach also config file, if it helps.

0 件の賞賛
返信

2,135件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @bora 

Can you see any active signal on pixel clock interface and data line? Can you measure the real pixel clock on board?
Is there any other parameter need to be added into panel-timing referring the panel spec?


Best Regards,
Zhiming

0 件の賞賛
返信

2,124件の閲覧回数
bora
Contributor II

Hi ,
When I measure LVDS pins, the voltages are 0 V. Panel timing parameter added based on display timing table.

0 件の賞賛
返信

2,602件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @bora 


The timing in dts can't be parsed. Please refer panel-lvds in other dts, like below dts node.

panel {
		compatible = "panel-lvds";
		width-mm = <170>;
		height-mm = <28>;
		data-mapping = "jeida-18";

		panel-timing {
			clock-frequency = <49500000>;
			hactive = <800>;
			hback-porch = <48>;
			hfront-porch = <312>;
			hsync-len = <40>;
			vactive = <600>;
			vback-porch = <19>;
			vfront-porch = <61>;
			vsync-len = <20>;
			hsync-active = <0>;
			vsync-active = <0>;
			de-active = <1>;
			pixelclk-active = <1>;
		};

		port {
			panel_out_bridge: endpoint {
				remote-endpoint = <&bridge_out_panel>;
			};
		};
	};




Best Regards,
Zhiming

0 件の賞賛
返信

2,595件の閲覧回数
bora
Contributor II
Thank you for that but I still have these failures:

0.876581] imx93-ldb ldb-display-controller: Failed to create device link (0x180) with 4ae30000.lcd-controller
[ 1.606293] imx93-ldb ldb-display-controller: Failed to create device link (0x180) with ldb-phy
[ 1.618237] imx93-ldb ldb-display-controller: Failed to create device link (0x180) with panel
0 件の賞賛
返信

2,576件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi,

These are noisy log, please ignore them.

To support a new LVDS panel, you need to modify the lcdif node.

&lcdif {
	assigned-clock-rates = <Pixel clock * 7>, <Pixel clock>, <400000000>, <133333333>;
};

Then modify the fracn_tbl in drivers/clk/imx/clk-fracn-gppll.c

PLL_FRACN_GP(455000000U, 151, 2, 3, 1, 8),



Best Regards,
Zhiming

0 件の賞賛
返信

2,570件の閲覧回数
bora
Contributor II
I modified lcdif
&lcdif {
status = "okay";
assigned-clock-rates = <42000000>, <6000000>, <400000000>, <133333333>;
};

and added
PLL_FRACN_GP(455000000U, 151, 2, 3, 1, 8), in the driver but with fb-test I dont see anything on the panel.
0 件の賞賛
返信

2,541件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @bora 

PLL_FRACN_GP(455000000U, 151, 2, 3, 1, is for Pixel clock=65MHz referring your original panel timing. Can you check and update your timing here?

Best Regards,
Zhiming

0 件の賞賛
返信

2,522件の閲覧回数
bora
Contributor II
I set it for 6.5MHz pixel clock and still didnt work. PLL_FRACN_GP(45500000U, 151, 2, 3, 1, 8). I can only set backlight
0 件の賞賛
返信

2,454件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi,

Why is the pixel clock here not 6.5 Mhz? If you define 6.5 MHz in the panel-simple/panel-timing node, then the lcdif device tree needs to be synchronized here as well.

assigned-clock-rates = <42000000>, <6000000>, <400000000>, <133333333>;

Best Regards,
Zhiming

0 件の賞賛
返信

2,139件の閲覧回数
bora
Contributor II

Hi,

I set it again 6.5Mhz and still doesnt work. I see /dev/fb0 and I attach config file, if it helps

0 件の賞賛
返信