imx93 debix_model_c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx93 debix_model_c

918 Views
AnkitaLengare24
Contributor II

I am trying to Burn M33 core. below the attache the elf file which we tryning run on the below path  but i am receving the eroor like,

root@DebixModelC:/# echo start > /sys/class/remoteproc/remoteproc0/state

-sh: echo: write error: Connection timed out

root@DebixModelC:/# echo offline > /sys/class/remoteproc/remoteproc0/state

-sh: echo: write error: Invalid argument

 

this below steps and cmds we are following

View status:-

cat /sys/class/remoteproc/remoteproc0/state

offline close:-

echo /home/root/freertos_hello.elf > /sys/class/remoteproc/remoteproc0/firmware

 

echo start > /sys/class/remoteproc/remoteproc0/state,when i hit this cmd it will take some time and give the error like,

-sh: echo: write error: Connection timed out

 

so why this error is showing , i think file is not compaitable or the version of the file is not supporting . that why error is showing

 

any one can faced this issue..........

0 Kudos
Reply
1 Reply

894 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to section "8.3.7 Using Linux remoteproc (i.MX 93 and i.MX 95)" in https://www.nxp.com.cn/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf

Please try the attached firmware file for i.mx93evk.

0 Kudos
Reply