imx93 cm33 flexio pwm disable output pin in the timer interrput

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx93 cm33 flexio pwm disable output pin in the timer interrput

806件の閲覧回数
lidafu
Contributor II

Hello,

I'm running an application on IMX93 CM33 core and I'm using FLEXIO as the PWM output.

The PWM signal is working good, but our application scenario requires PWM output stop at some certain conditions while re-enable.

Is it possible to enable/disable the PWM output while still keeping the FLEXIO timer running?

タグ(2)
0 件の賞賛
返信
1 返信

782件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer FlexIO PWM mode example code for i.MX93 via NXP Github.

You can set PWM working in idle status if duing application to disable PWM output.

PWM demo detailed info could check here

Wish it helps.

Mike

0 件の賞賛
返信