imx93 UUU starts uboot but dont execute fastboot commands

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx93 UUU starts uboot but dont execute fastboot commands

跳至解决方案
812 次查看
spawn
Contributor III

Hello,

I'm trying to boot and flash an imx93 using uuu, but it's not working.

Uboot starts but then uuu  does not seem to run fastboot commands to flash.

Run built-in script:                                
 uuu_version 0.0.1                                  
                                                    
# @_image                  | bootloader             
                                                                                                         
SDPS: boot -f x-u-boot.bin                                                                                                                                    
FB: ucmd mmc dev 0                                                                                       
FB: flash mmc0boot0 x-u-boot.bin                    
FB: done                                            
                                                                                                         
                                                                                                         
Wait for Known USB Device Appear...                                                                      
New USB Device Attached at 3:41-E5EA7500DEF94036                                                         
3:41-E5EA7500DEF94036>Start Cmd:SDPS: boot -f x-u-boot.bin                                                                                                    
100%3:41-E5EA7500DEF94036>Okay (4.759s) 

 Do you know why ?

ps: once uboot is running, if I run 'fastboot usb 0' , then I can use uuu to run the fastboot commands that did not seem to run before.

0 项奖励
回复
1 解答
805 次查看
spawn
Contributor III

I guess I have start fastboot automatically somehow.

在原帖中查看解决方案

0 项奖励
回复
1 回复
806 次查看
spawn
Contributor III

I guess I have start fastboot automatically somehow.

0 项奖励
回复