imx93 UUU starts uboot but dont execute fastboot commands

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx93 UUU starts uboot but dont execute fastboot commands

Jump to solution
818 Views
spawn
Contributor III

Hello,

I'm trying to boot and flash an imx93 using uuu, but it's not working.

Uboot starts but then uuu  does not seem to run fastboot commands to flash.

Run built-in script:                                
 uuu_version 0.0.1                                  
                                                    
# @_image                  | bootloader             
                                                                                                         
SDPS: boot -f x-u-boot.bin                                                                                                                                    
FB: ucmd mmc dev 0                                                                                       
FB: flash mmc0boot0 x-u-boot.bin                    
FB: done                                            
                                                                                                         
                                                                                                         
Wait for Known USB Device Appear...                                                                      
New USB Device Attached at 3:41-E5EA7500DEF94036                                                         
3:41-E5EA7500DEF94036>Start Cmd:SDPS: boot -f x-u-boot.bin                                                                                                    
100%3:41-E5EA7500DEF94036>Okay (4.759s) 

 Do you know why ?

ps: once uboot is running, if I run 'fastboot usb 0' , then I can use uuu to run the fastboot commands that did not seem to run before.

0 Kudos
Reply
1 Solution
811 Views
spawn
Contributor III

I guess I have start fastboot automatically somehow.

View solution in original post

0 Kudos
Reply
1 Reply
812 Views
spawn
Contributor III

I guess I have start fastboot automatically somehow.

0 Kudos
Reply