imx8x in big endian ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8x in big endian ?

3,383 Views
LaurentBardet
Contributor III

Hello,

For i.MX8X (QXP and others), can A35 cores be programmed in big-endian ?

ARMv8 documention says:

- instruction fetches are always treated as little-endian,

- data-access is  IMPLEMENTATION DEFINED whether both little-endian and big-little modes are supported (and if only one which one is supported is also IMPLEMENTATION DEFINED - here obviously little-endian).

Best regards,

Laurent

2 Replies

3,293 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Laurent,

ARM architecture itself indeed supports both big and small endianness. However, only little-endian implementations have been used and implemented on the i.MX8 processors to date. All software releases supported will use little endianness, which is the endianness currently supported.

The i.MX8X in is still in pre-production so some documentation may not be available. But on the available preliminary documentation you can see which interfaces provide endianness settings in case have your application requires it. For further technical information on this processor in pre-production status please refer to your FAE or Distributor.

My apologies for the inconvenience!

Regards,

3,293 Views
LaurentBardet
Contributor III

Thank you for your fast reply.

regards,

Laurent

0 Kudos
Reply