Hi,
We're using the i.MX8ULP for our product.
When suspending, we powerdown the M33 core as well as suspending on the A35 (as the power_mode_switch demo does with LPM_PowerModePowerDown)
My understanding of this mode of this mode is that wake-ups can only come from WUU0 in the demo, which can wake up for a variety of sources (LPTMR[0-1], gpios...)
My question here is that, is it possible to also use WUU1 in this case? (or perhaps WKPU)
I would like to also be able to wake up from PTE/PTF or USB PHY wakeup.
WUU1 is connected to PCC3 so I am not sure it is possible to use it directly from the M33 core (or if the M33 core would even get an interrupt in this case...), but I assume it could wake up the A35 core directly which would in turn be able to wake up the M33 core somehow? (I would have hoped for a WUU0 source being available from the mailbox but I do not see one...)
Unfortunately I've looked everywhere I could find (mcuxsdk examples, latest linux kernel) and could not find anything making use of the WUU1 or WKPU, and the documentation is rather sparse, so any help would be appreciated.
Thank you,
Dominique