imx8ulp falcon image cannot burn

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx8ulp falcon image cannot burn

跳至解决方案
2,245 次查看
tangchao90
Contributor III

my branch is scarthgap-6.6.36-2.1.0

https://github.com/nxp-imx/meta-imx/tree/scarthgap-6.6.36-2.1.0

https://github.com/nxp-imx-support/meta-imx-fastboot/tree/lf-6.6.36-2.1.0

my board is 

https://www.nxp.com/design/design-center/development-boards-and-designs/MCIMX8ULP-EVK?tid=vanimx8ulp...

According to the manual,MACHINE ??= 'imx8ulp-lpddr4-evk'  but the image can't burn,below is  the burn log. when i use branch imx_6.1.55_2.2.0, it can burn and start success,but i want to start quickly in falcon mode 

U-Boot SPL 2024.04+gde16f4f1722+p0 (Sep 02 2024 - 10:44:35 +0000)
Normal Boot
ELE firmware version 1.2.0-4b189593
upower_apd_inst_isr: entry
upower_init: soc_id=48
upower_init: version:11.11.13
upower_init: start uPower RAM service
user_upwr_rdy_callb: soc=b
user_upwr_rdy_callb: RAM version:12.18
Turning on switches...
Turn on switches ok
Turning on memories...
Turn on memories ok
Clearing DDR retention...
Clear DDR retention ok
SEC0: RNG instantiated
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###

标签 (1)
0 项奖励
回复
1 解答
2,089 次查看
tangchao90
Contributor III

my steps is below

1.  repo init -u https://github.com/nxp-imx/imx-manifest.git -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml

2. repo sync

3. enter the source directory and

 git clone -b lf-6.6.36-2.1.0 https://github.com/nxp-imx-support/meta-imx-fastboot

4. DISTRO=fsl-imx-wayland MACHINE=imx8ulpevk source imx-setup-release.sh -b build

5. cd build and 

bitbake-layers add-layer ../sources/meta-imx-fastboot

6. bitbake imx-image-full

but my imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33  file size is 1224KB

i download from  https://www.nxp.com/webapp/Download?colCode=L6.6.36_2.1.0_MX8ULP&appType=license imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33 file size is 1806KB

so my steps is not ok?

 

在原帖中查看解决方案

0 项奖励
回复
7 回复数
2,217 次查看
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @tangchao90 

I hope you are doing well.

 

Could you please clarify if you are following the AN14093?

Are you using other method?

 

Please, if possible share steps to reproduce the issue.

 

Best regards,

Salas.

0 项奖励
回复
2,125 次查看
tangchao90
Contributor III

my step is below:

1.  repo init -u https://github.com/nxp-imx/imx-manifest.git -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml

2. repo sync

3. enter the source directory and

 git clone -b lf-6.6.36-2.1.0 https://github.com/nxp-imx-support/meta-imx-fastboot

4. DISTRO=fsl-imx-wayland MACHINE=imx8ulp-lpddr4-evk source imx-setup-release.sh -b build

5. cd build and 

bitbake-layers add-layer ../sources/meta-imx-fastboot

6. bitbake imx-image-multimedia

after building , i can get image and burnin evk board

.\uuu.exe -b emmc_all .\imx-boot-imx8ulp-lpddr4-evk-sd.bin-flash_singleboot_m33 .\imx-image-multimedia-imx8ulp-lpddr4-evk.rootfs-20250124060345.wic

0 项奖励
回复
2,192 次查看
elena_popa
NXP Employee
NXP Employee

Hi @tangchao90 

Are you using UUU to flash the image? If so, please use the commands marked as a solutions in this ticket: https://community.nxp.com/t5/i-MX-Processors/How-to-load-Falcon-mode-image-to-emmc-on-imx8mplus-dev-... 

Thanks,

Elena

0 项奖励
回复
2,127 次查看
tangchao90
Contributor III

yes,  I use emmc flash and the command

.\uuu.exe -b emmc_all .\imx-boot-imx8ulp-lpddr4-evk-sd.bin-flash_singleboot_m33 .\imx-image-multimedia-imx8ulp-lpddr4-evk.rootfs-20250124060345.wic

uuu version is uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.182-0-ga561ed7

0 项奖励
回复
2,103 次查看
elena_popa
NXP Employee
NXP Employee

Hi @tangchao90 

The commands sequence should be:

.\uuu.exe -b emmc_all <default_bootloader> .\imx-image-multimedia-imx8ulp-lpddr4-evk.rootfs-20250124060345.wic

.\uuu.exe -b emmc <default_bootloader> <falcon_mode_bootloader>

The first uuu command writes the wic image using the default bootloader.

The second uuu command writes the bootloader with falcon mode enabled (<falcon_mode_bootloader>) using the default bootloader.

For easiness, you can take the default bootloader from here: https://www.nxp.com/webapp/Download?colCode=L6.6.36_2.1.0_MX8ULP&appType=license

 

Thanks,

Elena

0 项奖励
回复
2,084 次查看
tangchao90
Contributor III

oh , i understand you!  the <default_bootloader> is build without meta-imx-fastboot!

thank you

now my imx8ulp starts up with falcon image

0 项奖励
回复
2,090 次查看
tangchao90
Contributor III

my steps is below

1.  repo init -u https://github.com/nxp-imx/imx-manifest.git -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml

2. repo sync

3. enter the source directory and

 git clone -b lf-6.6.36-2.1.0 https://github.com/nxp-imx-support/meta-imx-fastboot

4. DISTRO=fsl-imx-wayland MACHINE=imx8ulpevk source imx-setup-release.sh -b build

5. cd build and 

bitbake-layers add-layer ../sources/meta-imx-fastboot

6. bitbake imx-image-full

but my imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33  file size is 1224KB

i download from  https://www.nxp.com/webapp/Download?colCode=L6.6.36_2.1.0_MX8ULP&appType=license imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33 file size is 1806KB

so my steps is not ok?

 

0 项奖励
回复