imx8ulp falcon image cannot burn

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8ulp falcon image cannot burn

ソリューションへジャンプ
2,168件の閲覧回数
tangchao90
Contributor III

my branch is scarthgap-6.6.36-2.1.0

https://github.com/nxp-imx/meta-imx/tree/scarthgap-6.6.36-2.1.0

https://github.com/nxp-imx-support/meta-imx-fastboot/tree/lf-6.6.36-2.1.0

my board is 

https://www.nxp.com/design/design-center/development-boards-and-designs/MCIMX8ULP-EVK?tid=vanimx8ulp...

According to the manual,MACHINE ??= 'imx8ulp-lpddr4-evk'  but the image can't burn,below is  the burn log. when i use branch imx_6.1.55_2.2.0, it can burn and start success,but i want to start quickly in falcon mode 

U-Boot SPL 2024.04+gde16f4f1722+p0 (Sep 02 2024 - 10:44:35 +0000)
Normal Boot
ELE firmware version 1.2.0-4b189593
upower_apd_inst_isr: entry
upower_init: soc_id=48
upower_init: version:11.11.13
upower_init: start uPower RAM service
user_upwr_rdy_callb: soc=b
user_upwr_rdy_callb: RAM version:12.18
Turning on switches...
Turn on switches ok
Turning on memories...
Turn on memories ok
Clearing DDR retention...
Clear DDR retention ok
SEC0: RNG instantiated
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###

ラベル(1)
0 件の賞賛
返信
1 解決策
2,012件の閲覧回数
tangchao90
Contributor III

my steps is below

1.  repo init -u https://github.com/nxp-imx/imx-manifest.git -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml

2. repo sync

3. enter the source directory and

 git clone -b lf-6.6.36-2.1.0 https://github.com/nxp-imx-support/meta-imx-fastboot

4. DISTRO=fsl-imx-wayland MACHINE=imx8ulpevk source imx-setup-release.sh -b build

5. cd build and 

bitbake-layers add-layer ../sources/meta-imx-fastboot

6. bitbake imx-image-full

but my imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33  file size is 1224KB

i download from  https://www.nxp.com/webapp/Download?colCode=L6.6.36_2.1.0_MX8ULP&appType=license imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33 file size is 1806KB

so my steps is not ok?

 

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
2,140件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @tangchao90 

I hope you are doing well.

 

Could you please clarify if you are following the AN14093?

Are you using other method?

 

Please, if possible share steps to reproduce the issue.

 

Best regards,

Salas.

0 件の賞賛
返信
2,048件の閲覧回数
tangchao90
Contributor III

my step is below:

1.  repo init -u https://github.com/nxp-imx/imx-manifest.git -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml

2. repo sync

3. enter the source directory and

 git clone -b lf-6.6.36-2.1.0 https://github.com/nxp-imx-support/meta-imx-fastboot

4. DISTRO=fsl-imx-wayland MACHINE=imx8ulp-lpddr4-evk source imx-setup-release.sh -b build

5. cd build and 

bitbake-layers add-layer ../sources/meta-imx-fastboot

6. bitbake imx-image-multimedia

after building , i can get image and burnin evk board

.\uuu.exe -b emmc_all .\imx-boot-imx8ulp-lpddr4-evk-sd.bin-flash_singleboot_m33 .\imx-image-multimedia-imx8ulp-lpddr4-evk.rootfs-20250124060345.wic

0 件の賞賛
返信
2,115件の閲覧回数
elena_popa
NXP Employee
NXP Employee

Hi @tangchao90 

Are you using UUU to flash the image? If so, please use the commands marked as a solutions in this ticket: https://community.nxp.com/t5/i-MX-Processors/How-to-load-Falcon-mode-image-to-emmc-on-imx8mplus-dev-... 

Thanks,

Elena

0 件の賞賛
返信
2,050件の閲覧回数
tangchao90
Contributor III

yes,  I use emmc flash and the command

.\uuu.exe -b emmc_all .\imx-boot-imx8ulp-lpddr4-evk-sd.bin-flash_singleboot_m33 .\imx-image-multimedia-imx8ulp-lpddr4-evk.rootfs-20250124060345.wic

uuu version is uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.182-0-ga561ed7

0 件の賞賛
返信
2,026件の閲覧回数
elena_popa
NXP Employee
NXP Employee

Hi @tangchao90 

The commands sequence should be:

.\uuu.exe -b emmc_all <default_bootloader> .\imx-image-multimedia-imx8ulp-lpddr4-evk.rootfs-20250124060345.wic

.\uuu.exe -b emmc <default_bootloader> <falcon_mode_bootloader>

The first uuu command writes the wic image using the default bootloader.

The second uuu command writes the bootloader with falcon mode enabled (<falcon_mode_bootloader>) using the default bootloader.

For easiness, you can take the default bootloader from here: https://www.nxp.com/webapp/Download?colCode=L6.6.36_2.1.0_MX8ULP&appType=license

 

Thanks,

Elena

0 件の賞賛
返信
2,007件の閲覧回数
tangchao90
Contributor III

oh , i understand you!  the <default_bootloader> is build without meta-imx-fastboot!

thank you

now my imx8ulp starts up with falcon image

0 件の賞賛
返信
2,013件の閲覧回数
tangchao90
Contributor III

my steps is below

1.  repo init -u https://github.com/nxp-imx/imx-manifest.git -b imx-linux-scarthgap -m imx-6.6.36-2.1.0.xml

2. repo sync

3. enter the source directory and

 git clone -b lf-6.6.36-2.1.0 https://github.com/nxp-imx-support/meta-imx-fastboot

4. DISTRO=fsl-imx-wayland MACHINE=imx8ulpevk source imx-setup-release.sh -b build

5. cd build and 

bitbake-layers add-layer ../sources/meta-imx-fastboot

6. bitbake imx-image-full

but my imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33  file size is 1224KB

i download from  https://www.nxp.com/webapp/Download?colCode=L6.6.36_2.1.0_MX8ULP&appType=license imx-boot-imx8ulpevk-sd.bin-flash_singleboot_m33 file size is 1806KB

so my steps is not ok?

 

0 件の賞賛
返信